Introducing the TI-Nspire CX II
It's a big day for Texas Instruments. Today, we introduced the all-new TI-Nspire CX II family of graphing calculators, bringing a 2 ½ times faster processor, an updated, new look and added math and coding features that will help bring STEM (science, technology, engineering and math) subjects to life for students. Building on the popular TI-Nspire CX line of graphing calculators, the new TI-Nspire CX II and TI-Nspire CX II CAS give students more opportunities to visualize important, abstract concepts, not just in math class, but in science and computer programming courses.
"Students and teachers asked us to make their graphing calculator more responsive as they are using it increasingly to explore an array of complex, STEM concepts,"
Peter Balyta, Ph.D., president of TI Education Technology
“Students and teachers asked us to make their graphing calculator more responsive as they are using it increasingly to explore an array of complex, STEM concepts,” said Peter Balyta, Ph.D., president of TI Education Technology. “Once teachers experience the new TI-Nspire CX II, they will immediately appreciate the improved visuals on the screen, added power and robust, new features that help students explore STEM.”
Teachers will also appreciate that the key placement, navigation and computer menus are the same as earlier TI-Nspire models so they can continue to use their current classroom lessons. Parents will appreciate that a one-time purchase of a TI-Nspire CX II or CX II CAS will take students through all of their math and science courses in middle school, high school and college– everything from chemistry to calculus and can even help them learn to code.
The TI-Nspire CX II graphing calculator is allowed on high-stakes exams, including the PSAT/NMSQT*, SAT* and ACT® college entrance exams as well as Advanced Placement* and IB® exams that allow or require a graphing calculator. The TI-Nspire CX II and CX II CAS will be available for purchase at major retail stores in time for back to school 2019. For information on availability, visit our website: education.ti.com/TI-Nspire-CXII.
TI-Nspire CX II Specifications and Features:
- Color, backlit display
- Screen size: 320 x 240 pixels (3.5" diagonal)
- Screen resolution: 125 DPI; 16-bit color
- Powered by the TI-Rechargeable Battery (included)
- USB port for computer connectivity
- 90 MB storage memory / 64MB operating memory
- 396 MHz processor speed
- Additional technical specifications are available online at education.ti.com/TI-Nspire-CXII
SAT* and AP*are registered trademarks of the College Entrance Examination Board
PSAT/NMSQT* is a registered trademark of the College Board and the National Merit Scholarship Corporation
IB is a registered trademark owned by the International Baccalaureate Organization
About the author: Ellen Fishpaw is the Media Relations and Communications Manager for Texas Instruments Education Technology. Before joining TI five years ago, Ellen was a broadcast journalist for 13 years, working at television stations across the country, from North Carolina to New Mexico. She most recently worked for NBC 5 in Dallas as a crime reporter before hanging up the microphone for a TI-84 Plus CE. Follow her on Twitter @ellenfishpaw.
.Tagcloud