Summer of STEM: Egg in a Bottle
Posted 06/27/2018 by Erick Archer
How can you get a hard-boiled egg inside of a milk bottle without pushing it?
What you’ll need:- Milk bottle or equivalent with an opening diameter of about 2.5” to 3”
- Small to medium hard-boiled egg
- Cooking oil
- Matches or a lighter
- 3” x 3” piece of paper
- Coat the opening of the bottle with cooking oil to decrease friction.
- Loosely roll the piece of paper and light it with the match or lighter, being careful not to burn yourself.
- Drop the lit paper into the bottle and quickly but gently, place the egg onto the bottle opening on one end or the other.
- Watch the egg get sucked into the bottle.
- The burning paper quickly heats the air inside the bottle, causing an expansion of air inside the bottle.
- That warm air pushes out through the top of the bottle and past the egg.
- Because the fire burns up the oxygen inside the bottle quickly, and the egg is acting to stop any incoming air by acting as a seal, the air pressure inside the bottle quickly becomes less than the air pressure outside the bottle and above the egg.
- The difference in air pressure between the inside and outside causes the egg to get pushed into the bottle!
- Notice the paper probably didn’t burn all the way. That is because the rate of incoming air was too small (due to the egg blocking the opening), and the fire went out since there was no more oxygen to burn inside the bottle.
- To remove the egg without destroying it or the bottle, invert the bottle so you can get the remaining paper out. Then, invert it fully so the egg is in the opening. Put your mouth on the opening and blow hard while keeping the bottle inverted. After a quick puff, remove your mouth to allow the egg to escape … otherwise you will be eating egg.☹️
Below, see a video of this experiment and others in action:
Tags:
Tagcloud
Archive
- 2026
- 2025
- 2024
- 2023
- 2022
-
2021
- January (1)
- February (2)
- March (5)
-
April (7)
- Top Tips for Tackling the SAT® with the TI-84 Plus CE
- Monday Night Calculus With Steve Kokoska and Tom Dick
- Which TI Calculator for the SAT® and Why?
- Top Tips From a Math Teacher for Taking the Online AP® Exam
- Celebrate National Robotics Week With Supervised Teardowns
- How To Use the TI-84 Plus Family of Graphing Calculators To Succeed on the ACT®
- AP® Statistics: 6 Math Functions You Must Know for the TI-84 Plus
- May (1)
- June (3)
- July (2)
- August (5)
- September (2)
-
October (4)
- Transformation Graphing — the Families of Functions Modular Video Series to the Rescue!
- Top 3 Halloween-Themed Classroom Activities
- In Honor of National Chemistry Week, 5 “Organic” Ways to Incorporate TI Technology Into Chemistry Class
- 5 Spook-tacular Ways to Bring the Halloween “Spirits” Into Your Classroom
- November (4)
- December (1)
- 2020
- 2019
-
2018
- January (1)
- February (5)
- March (4)
- April (5)
- May (4)
- June (4)
- July (4)
- August (4)
- September (5)
- October (8)
-
November (8)
- Testing Tips: Using Calculators on Class Assessments
- Girls in STEM: A Personal Perspective
- 5 Teachers You Should Be Following on Instagram Right Now
- Meet TI Teacher of the Month: Katie England
- End-of-Marking Period Feedback Is a Two-Way Street
- #NCTMregionals Kansas City 2018 Recap
- Slope: It Shouldn’t Just Be a Formula
- Hit a high note exploring the math behind music
- December (5)
- 2017
- 2016
- 2015