Education Technology

Knowledge Base Search

< Previous | 1125 - 1150 of 1414 results |  Next >

Solution 11380: Engineering Applications for the TI-89 Family and Voyage™ 200 Graphing Calculators.

...fty-seven (57) analytical routines solve problems in areas such as Steam Tables, Thermocouples, Section Properties, and Efflux. An interactive reference table provides data tables for Refrigerants, Water Properties, Laplace and Fourier Transforms, and Fuels and Combustion Properties. EE*Pro® App...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/general-information/11380

Solution 39417: Performing English/Metric Conversions on the TI-36X Solar.

...ish/Metric conversions on the TI-36X Solar? To perform English to Metric conversions on the TI-36X Solar please follow the example below: Convert 254 centimeters to inches: • Enter 254 • Press [2nd] then [>in] which is the second function of the 1 key. The screen should display 100 To reverse thi...
https://education.ti.com/en/customer-support/knowledge-base/scientific-elem-calculators/product-usage/39417

Solution 34293: Computing Binomialcdf on the TI-36X Pro.

...36X Pro? Binomialcdf computes a cumulative probability at x for the discrete binomial distribution with the specified numtrials and probability of success (p) on each trial. x can be nonnegative integer and can be entered with options of SINGLE, LIST or ALL (a list of cumulative probabilities is ...
https://education.ti.com/en/customer-support/knowledge-base/scientific-elem-calculators/product-usage/34293

Solution 12325: Troubleshooting a Two-line Display Scientific Calculator that Will Not Turn On.

...ill fail to power on. Follow the steps below to reset the calculator: 1) Hold down [CLEAR] and [ON] key at the same time. 2) Release both keys. 3) Once the keys have been released, the calculator should display a blinking cursor. Please Note: If the blinking cursor is not displayed, press the [O...
https://education.ti.com/en/customer-support/knowledge-base/scientific-elem-calculators/troubleshooting-messages-unexpected-results/12325

Solution 36735: Resolving the Error "FRQ DOMAIN Error" on the TI-30X IIB / TI-30X IIS Scientific Calculators.

...IIB / TI-30X IIS scientific calculators? The error message "FRQ DOMAIN Error" indicates that one of the frequency entries for a statistics problem exceeds the maximum number allowed.  The maximum value for a frequency value is 99. To resolve this issue please follow the steps below: • Push the...
https://education.ti.com/en/customer-support/knowledge-base/scientific-elem-calculators/troubleshooting-messages-unexpected-results/36735

Solution 12078: Comparison Between the TI-89 Titanium and the TI-89.

...Titanium offers 3 times the memory of the TI-89 for Calculator Software Applications (Apps), 16 preloaded Apps (compared to 5 on the TI-89) including CellSheet™ App, NoteFolio™ App, and EE*Pro®, a built-in USB port for connectivity, and a USB cable with every unit. For more information, please v...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/general-information/12078

Solution 12298: Texas Instruments Calculators that Display Results with Remainders.

... Knowledge Base Search Does Texas Instruments have a calculator that will display an answer in remainder form? The TI-34 II Explorer Plus™, TI-10, TI-15, TI-34 MultiView™ and TI-73 calculators have the ability to display results with remainders. Refer to the examples provided bel...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/general-information/12298

Solution 27470: Issues following example Time-Value-of- Money Function in the TI-89 Titanium and Voyage 200 Guidebooks

... titled "Time-Value-of- Money Function" in both the TI-89 Titanium and Voyage 200 Guidebooks has a typo. The example listed in the guidebook lists spaces where multiplication signs are supposed to be listed. The corrected instructions are listed below: tvm(temp1,temp2,temp3,temp4,temp5,temp6) Fun...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/troubleshooting-messages-unexpected-results/27470

Solution 15420: Correcting the Error "Equation Length" on the TI-30X IIS/B and TI-30XS/TI-30XB MultiView™ Scientific Calculators.

...or "Equation Length" on the TI-30X IIS/B and TI-30XS/TI-30XB MultiView scientific calculators? The error "Equation Length" indicates that the entry exceeds the maximum number of digits allowed in the entry line for statistics or a constant entry line. • For the TI-30X IIS/B, the maximum number of...
https://education.ti.com/en/customer-support/knowledge-base/scientific-elem-calculators/troubleshooting-messages-unexpected-results/15420

Solution 22230: Resolving the Error "Insufficient Memory" When Transferring Data to a TI-89 Family, TI-92 Family, or Voyage™ 200.

...Voyage 200 and there is not enough RAM memory to transfer the complete data, the "Insufficient Memory" error will appear. All calculators must have a certain amount of RAM available so that they can perform their various functions. If this message is displayed users will need to delete any unused...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/troubleshooting-messages-unexpected-results/22230

Solution 15889: Correcting the Message "ERROR" on the TI-36X Solar.

... Why is my TI-36X Solar displaying the message "Error" and how can I correct it? When "Error" appears on the display, the calculator will not accept a keyboard entry. Press the [CE/C] to clear the error condition. Press the [CE/C] twice to clear the condition and all pending operations. The...
https://education.ti.com/en/customer-support/knowledge-base/scientific-elem-calculators/troubleshooting-messages-unexpected-results/15889

Solution 25490: What is the Ohio Gradualtion Test (OGT) Red Calculator and why is it referred to as the TI-30XIISR?

...lution 25490: What is the Ohio Gradualtion Test (OGT) Red Calculator and why is it referred to as the TI-30XIISR? Texas Instruments has produced a red TI-30X IIS specifically for the state of Ohio to use for their Ohio Graduation Tests (OGT).  These schools refer to it as the TI-30XIISR....
https://education.ti.com/en/customer-support/knowledge-base/scientific-elem-calculators/general-information/25490

Solution 18209: Using the Hyperbolic Functions on the TI-30X IIS/B and TI-30XS MultiView™.

...S/B and TI-30XS MultiView? Hyperbolic functions are analogs of regular trig functions, or better known as circular functions. Press [2nd] [HYP] to access the hyperbolic function (sinh, cosh, tanh) of the trig function to be used. Hyperbolic calculations are not affected by the mode of the calcul...
https://education.ti.com/en/customer-support/knowledge-base/scientific-elem-calculators/product-usage/18209

Solution 18729: Performing Metric Conversions on the TI-36X II.

... do I perform metric conversions on the TI-36X II? The TI-36X II has a menu with 20 conversions from the metric system into the English system and vice versa. To access this menu press [Conver] and scroll to the selected conversion and press [ENTER]. To reverse the conversion press [2nd] while t...
https://education.ti.com/en/customer-support/knowledge-base/scientific-elem-calculators/product-usage/18729

Solution 11870: Using Solve( with Trigonometric Functions Returns Unexpected Results on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.

...mily, and Voyage 200 are showing that this equation has an infinite set of solutions by displaying @n1*p. The integer suffix of "@n" increases for successive problems, then wraps back to 1 after 255. "@n" is the units representation of an "arbitrary integer." Please see the TI-89 family, TI-92 fa...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/troubleshooting-messages-unexpected-results/11870

Solution 10441: Resolving ERROR 13 DIMENSION or ERROR 12 DIM MISMATCH Message on the TI-86.

... 12 DIM MISMATCH is the result of one or more stat plots being selected when not using the stat plots feature of the TI-86. The following key sequence can be used to turn the stat plots off:  1) [2nd] [STAT]  2) [F3]  3) [F5]  4) [ENTER] This will turn all plots off and should allow for norma...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/troubleshooting-messages-unexpected-results/10441

Solution 22310: Correcting the Error Message Variable is Locked, Protected, or Archived on the TI-89 Family, TI-92 Family and Voyage™ 200.

...en attempting to delete a locked program, equation, list, etc. from the var-link menu using a TI-89 family, TI-92 family or Voyage 200 calculator. Since the item to be deleted is locked,  then the user will not be able to remove it from the unit. To unlock the item and delete it, please see the...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/troubleshooting-messages-unexpected-results/22310

Solution 29030: Input is Returned as the Solution After Pressing the [enter] Key When Using the TI-36X Pro Scientific Calculator.

...ut as the solution? The TI-36X Pro scientific calculator has built-in functionality called "MathPrint" which is similar to what is found on the TI-84 Plus family and TI-Nspire family handhelds. MathPrint allows the calculator to display input and output in symbolic or exact form such as: √11 is d...
https://education.ti.com/en/customer-support/knowledge-base/scientific-elem-calculators/product-usage/29030

Solution 16409: Correcting a TI-89 Family, TI-92 Family, or Voyage™ 200 Graphing Calculator That is Locked Displaying "Busy" for a Prolonged Period of Time.

...ly or Voyage 200 graphing calculator for over 10 minutes? The TI-89 family, TI-92 family or Voyage 200 graphing calculators may display "busy" for a certain time while processing complex computations or solving equations. However, if the calculator displays busy for more than 10 minutes please s...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/troubleshooting-messages-unexpected-results/16409

Solution 30130: When Using Symbolic Pi, Mixed Number Conversions are Improperly Displayed on the TI-36X Pro and TI-30X Pro MultiView™ Calculators.

...ro MultiView calculator? Issue: When you do a calculation using symbolic pi, you will get an approximate decimal answer to the number of decimal places carried by a calculator. If you convert the decimal result (stored in the calculator) to a mixed number and then repeatedly toggle back and for...
https://education.ti.com/en/customer-support/knowledge-base/scientific-elem-calculators/product-usage/30130

Solution 12151: Updating to Operating System (OS) Version 3.10 for the TI-89 Titanium and Voyage™ 200 Deletes All Calculator Software Applications (Apps).

...10 on the TI-89 Titanium or Voyage 200? The TI-89 Titanium and Voyage 200 OS v3.10 will reset the RAM and Flash ROM memory as part of the updating process. This is done to ensure maximum compatibility with the operating system and apps. It is highly recommended that existing programs and apps are...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/troubleshooting-messages-unexpected-results/12151

Solution 12074: Troubleshooting a TI-89 that Displays Line 1111 Emulator.

... level machine code error usually generated by errant assembly code. If Line 1111 Emulator is displayed, the calculator must be reset. The reset procedure will delete all the items that are in the memory of the graphing calculator. Use the reset procedure below: 1) Press and hold the [2nd] key...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/troubleshooting-messages-unexpected-results/12074

Solution 34073: Inputting Exponents Using the TI-36X Pro Scientific Calculator.

...g the TI-36X Pro use [x[]].Example: 34• Press [3] [X[]].• Press [4] [enter].• The answer is 81.When inputting exponents for a negative value, it is necessary to put parentheses around the negative value. If parentheses are not used, the calculator will evaluate it differently.Example: -44• Press ...
https://education.ti.com/en/customer-support/knowledge-base/scientific-elem-calculators/product-usage/34073

Solution 10617: ERROR SINGULARITY Using the Equation Solver on the TI-85 and TI-86 When a Solution is Calculated Using the TI-89 Family.

... "ERROR SINGULARITY" occurs when the SOLVER equation contains a singularity (a point at which the function is not defined). The difference between the software on the TI-89 family, TI-92 family and Voyage™ 200 and the TI-85 and TI-86 is that they use different linear system solvers,...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/troubleshooting-messages-unexpected-results/10617