Education Technology

Solution 15420: Correcting the Error "Equation Length" on the TI-30X IIS/B and TI-30XS/TI-30XB MultiView™ Scientific Calculators.

How can I correct the error "Equation Length" on the TI-30X IIS/B and TI-30XS/TI-30XB MultiView scientific calculators?

The error "Equation Length" indicates that the entry exceeds the maximum number of digits allowed in the entry line for statistics or a constant entry line.

• For the TI-30X IIS/B, the maximum number of digits to enter in the entry line is 88 digits.
• For the TI-30XS/TI-30XB MultiView, the maximum number of digits to enter in the entry line is 80 digits
• For both model calculators, the maximum number of statistics entries is 47.

NOTE: Combining an entry with a constant may make the entry exceed the limit.

Please see the TI-30X IIS/B and TI-30XS/TI-30XB MultiView guidebooks for additional information.