Education Technology

Solution 39417: Performing English/Metric Conversions on the TI-36X Solar.

How do I perform English/Metric conversions on the TI-36X Solar?

To perform English to Metric conversions on the TI-36X Solar please follow the example below:

Convert 254 centimeters to inches:

• Enter 254
• Press [2nd] then [>in] which is the second function of the 1 key.

The screen should display 100

To reverse this calculation and convert 100 inches to centimeters:

• Enter 100
• Press [3rd] then [>cm] which is the third function of the 1 key.

The display should read 254.

Please see the TI-36X Solar guidebook for additional information and full listing of available conversions.