Education Technology

Knowledge Base Search

< Previous | 125 - 150 of 1765 results |  Next >

Solution 34655: Using the RandInt() Function on the TI-84 Plus CE and TI-84 Plus C Silver Edition.

...ing the steps in KB#34503. The randInt() function generates and displays a random integer within a range specified by lower and upper integer bounds for a specified number of trials. The syntax for the randInt() function is listed below. randInt( lower,upper[,number of trials]) Example: Find t...
https://education.ti.com/en/customer-support/knowledge-base/ti-83-84-plus-family/product-usage/34655

Solution 38875: Asm84CEPrgm command is not accessible in catalog of the latest version of the TI-84 Plus CE Operating System.

... the "Asm84CEPrgm" command was disabled with the latest update to the TI-84 Plus CE graphing calculator Operating System. I will be glad to provide information on this subject.  There are classroom exams and other test scenarios where simple calculator clearing or calculator resets are used inste...
https://education.ti.com/en/customer-support/knowledge-base/ti-83-84-plus-family/product-usage/38875

Solution 37041: Taking screenshots from the TI-84 Plus family of calculators and saving them as image files using TI Connect CE

...E Software Connect your calculator to the computer’s USB port; turn the calculator on, by pressing the [ON] button; and make sure the calculator appears in the Content Panel. Select the Screen Capture workspace from the TI Connect™ CE software Workspace Panel on the left. Display t...
https://education.ti.com/en/customer-support/knowledge-base/ti-83-84-plus-family/product-usage/37041

Solution 37038: Backup and restore TI-84 Plus family graphing calculator files to a computer using TI Connect CE™ software.

...) Drag the file(s) to the Calculator List Panel, and hover over the desired connected calculator. 6) Release the mouse button when you see “+Copy” 7) For calculator image files, select a file name from the drop-down menu. This will be the name of the image on your calculator. Click “Send.”  Warni...
https://education.ti.com/en/customer-support/knowledge-base/ti-83-84-plus-family/product-usage/37038

Solution 11576: Algorithm Used for Calculating the Sine Regression On the TI-86, TI-83 Family, or TI-84 Plus Family.

...to calculate the sine regression on a TI-86, TI-83 family, or TI-84 Plus family? Sine regression on the TI-86, TI-83 family, or TI-84 Plus family, accepts as an input an (x,y) pair list for the independent and dependent variables respectively. The algorithm assumes that the kth (x,y) data pairs ...
https://education.ti.com/en/customer-support/knowledge-base/ti-83-84-plus-family/product-usage/11576

Solution 34420: Performing T-Test Computations Using the TI-83 Plus and TI-84 Plus Family of Graphing Calculators.

...form a T-Test calculation.  Data for this example: {30.3, 30.5, 30.6, 31, 30.7, 30.7, 30.4, 30.9, 31} Entering the data: 1) Press [STAT] [1] to access the STAT List Editor. 2) Input the example data into the L1 list, pressing the [ENTER] key after each entry. 3) Press [2nd] [MODE] to QUIT th...
https://education.ti.com/en/customer-support/knowledge-base/ti-83-84-plus-family/product-usage/34420

Solution 36979: "Unknown device" displays when I connect my TI-84 Plus family graphing calculator to the TI-Connect CE™ software

...on are connected to the TI-Connect CE software TI Connect CE will display them as an "Unknown device".  TI Connect CE only supports 2.55 OS and above for the TI-84 Plus family. Note: The TI-Nspire™ Handheld in TI-84 Plus Mode will also display as "Unknown device", TI Connect (v4.0) is the recomme...
https://education.ti.com/en/customer-support/knowledge-base/ti-83-84-plus-family/product-usage/36979

Solution 12085: Apps Icon Desktop Setting and Clock Functionality for the TI-89 or TI-92 Plus.

...he Voyage™ 200. Please note that the clock will only work on units whose About screens read Hardware Version 2.00. The About screen may be found by accessing the calculator's Home screen then pressing F1 Tools, and choosing A: About. For additional instructions on performing matrix operations, re...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/12085

Solution 12048: Changing the Scale of a Graph in The Geometer's Sketchpad® App for the TI-89 Family, TI-92 Plus and Voyage™ 200 Graphing Calculators.

...o change the scale of a graph in The Geometer's Sketchpad® App, please follow the steps listed below. For TI-89 Family users: • Press [2nd] [F1] to access the F6 menu. Select 4: Show Grid.• Move the arrow to select point (1,0). (1,0) is just an example and any other point can be used, if preferre...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/12048

Solution 23550: Performing Laplace and Inverse Laplace Transformations on the TI-89 Family, TI-92 Plus, Voyage™ 200 Graphing Calculators.

...Instruments graphing calculators do not have a built in function to perform laplace or inverse laplace transformations. However, with the addition of applications such as ME*Pro (designed for mechanical engineering) or EE*Pro (designed for electrical engineering) one can add this functionality. T...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/23550

Solution 34672: Graphing the Fibonacci Sequence on the TI-83 Plus and TI-84 Plus Family of Graphing Calculators.

...procedure below to graph the Fibonacci sequence: 1) Press [mode] 2) Press [↓] [↓] [↓] [→] [→] [→] to select SEQ and press [enter] 3) Press [Y=]. 4) For nMin= press [↑] [1] [enter] 5) For u(n)= press [2nd] [7] [ ( ] [X,T,θ,n] [-] [1] [ ) ] [+] [2ND] [7] [ ( ] [X,T,θ,n] [-] [2] [ ) ] [enter] 6) F...
https://education.ti.com/en/customer-support/knowledge-base/ti-83-84-plus-family/product-usage/34672

Solution 34611: Computing One Way Analysis of Variance (ANOVA) on the TI-83 Plus and TI-84 Plus Family of Graphing Calculators.

...veled by the three brands of balls. In this case, the null hypothesis cannot be rejected. Please see the TI-83 Plus and TI-84 Plus Family guidebooks for additional information. Last updated: 7/24/2023 Solution 34611: Computing One Way Analysis of Variance (ANOVA) on the TI-83 Plus and TI-84 Plu...
https://education.ti.com/en/customer-support/knowledge-base/ti-83-84-plus-family/product-usage/34611

Solution 34603: Finding the X-Intercept of a Function on the TI-83 Plus and TI-84 Plus Family of Graphing Calculators.

...3 Plus and TI-84 Plus family of graphing calculators? To find the x-intercepts of a function, the zero command must be used. Follow the example below for help with using the zero command. Example: 2X - 7 1) Press [Y=] to access the Y= Editor. 2) Press [Clear] then [2] [X,T,θ,n] [-] [7] 3) Pres...
https://education.ti.com/en/customer-support/knowledge-base/ti-83-84-plus-family/product-usage/34603

Solution 34814: Correcting a Data Type Error when Attaching a Distribution Formula to a List on the TI-83 Plus and TI-84 Plus Family of Graphing Calculators.

...to the L1 list. L2=normalcdf( -1E99, 200, L1*.9, L1*.9*.1) Some of the distribution functions, such as Normalpdf and Normalcdf, are not designed to accept lists as valid parameters. These two functions are designed to only accept floating numbers or integers. The same issue can easily be recreat...
https://education.ti.com/en/customer-support/knowledge-base/ti-83-84-plus-family/product-usage/34814

Solution 34777: Graphing a Non-Recursive Sequence on the TI-83 Plus and TI-84 Plus Family of Graphing Calculators.

... sequence is a sequence in which the nth term is a function of the independent variable n and each term is independent of all the other terms. NOTE: For this example, the handheld's mode settings will need to be changed. • Press [MODE]. • Scroll down and over to SEQ and press [ENTER] to change ...
https://education.ti.com/en/customer-support/knowledge-base/ti-83-84-plus-family/product-usage/34777

Solution 37718: Cannot restore the main application window after minimizing the Screen Capture window while open and in view on TI-Smartview CEfor Mac®.

...tview CEfor Mac®. website Home | Computer Software, iPad and Chrome Apps Knowledge Base Knowledge Base Search Why can I not restore the main application window after minimizing the ...
https://education.ti.com/en/customer-support/knowledge-base/sofware-apps/troubleshooting-messages-unexpected-results/37718

Solution 13481: Correcting the Error Message "The Wizard Could Not Find the Necessary Software" When Using the TI Connectivity Standard Mini-A to Mini-B USB Cable for Windows®/Mac® or the TI Connectivity Cable USB for Windows® /Mac® (silver).

...e tab. • Click the Device Manager button. • Look under Universal Serial Bus Controllers for either Unknown Device, or for the calculator's model (ex. TI-84 Plus, TI-89 Titanium) and right-click on the device. • Click the radio button next to "Install from a list or specific location (Advanced)" N...
https://education.ti.com/en/customer-support/knowledge-base/sofware-apps/troubleshooting-messages-unexpected-results/13481

Solution 11250: Repair/Service Availability for BAII PLUS™ Overhead Calculators.

...verhead units (available through the Finance Educator Support Program).For any BAII PLUS overhead calculators requiring service, please download an application or apply online at the Finance Educator Support Program. Since the Educator Support Program has replaced the BAII PLUS overhead unit ...
https://education.ti.com/en/customer-support/knowledge-base/financial-calculators/general-information/11250

Solution 15086: Updating the Emulated TI-84 Plus Family Operating System in TI-SmartView™ Emulator software

...us OS file onto the computer's desktop.2) Open the TI-SmartView 4.0 emulator software and click [View] [Graphing Calculator Model] [TI-84 Plus] to place the emulator in TI-84 Plus mode.3) Click [File] [Load File].4) Navigate to the computer's desktop and locate the OS file.5) Double-click on the ...
https://education.ti.com/en/customer-support/knowledge-base/sofware-apps/product-usage/15086

Solution 28493: Calculating the Reduced Row Echelon Form (rref) of a Matrix Using the TI-Nspire™ Family Products.

...orm of a matrix using the TI-Nspire family products? To calculate the reduced row echelon form of a matrix using the TI-Nspire family, the Calculator Application and "rref( )" command must be used. For an example, follow the steps below.   1) Press [home] and insert the Calculator Application. 2...
https://education.ti.com/en/customer-support/knowledge-base/ti-nspire-family/product-usage/28493

Solution 14849: Using a TI-84 Plus Family Calculator to Control TI-SmartView™ Emulator Software.

... Plus with the TI-SmartPad App can however control the TI-SmartView 4.0 emulator while in TI-84 C Silver Edition Emulator Mode. If using TI-Smartview CE emulator software you will need to download the TI-84 Plus CE SmartPad™ CE App. 1) Start TI-SmartView and connect the calculator to the computer...
https://education.ti.com/en/customer-support/knowledge-base/sofware-apps/product-usage/14849

Solution 40347: Tip Sheet for Implementation of Texas Instruments Account Based Licenses.

...ps for implementing Texas Instruments Account Based Licenses? The information below covers some common questions and best practices in setting up the TI-84 Plus CE App for Chrome OS for use by your teachers and students. For complete directions, please visit our OrgAdmin License and Entitlement M...
https://education.ti.com/en/customer-support/knowledge-base/sofware-apps/computer-software-installation-activation/40347

Solution 40465: Key Steps for Adding Teachers and Students to TI Account Based Software License.

...o your users. US chart TI Software Type of software Link to access TI-84 Plus CE online calculator Browser-based (Google Chrome browser) 84PlusCE.ti.com ...
https://education.ti.com/en/customer-support/knowledge-base/sofware-apps/computer-software-installation-activation/40465

Solution 40454: Process to “Renew” or “Extend” a Subscription for TI Software or Online Calculator

... “extended": TI-SmartView CE emulator software TI-Nspire CX Premium Teacher Software TI-Nspire CX CAS Student Software TI-Nspire CX Student Software TI-84 Plus CE online calculator TI-Nspire CX II online calculator To continue to use the above products after the subscription period expires, a ne...
https://education.ti.com/en/customer-support/knowledge-base/sofware-apps/computer-software-installation-activation/40454

Solution 34429: Finding the Row Echelon Form on the TI-83 Plus and TI-84 Plus Family of Graphing Calculators.

... exit the matrix editor, and then paste the ref() function on the home screen with the name of the matrix. The example below will demonstrate this procedure. Example: Find the ref() of matrix [A] Solution: To enter the matrix: • Press [2nd] [MATRIX]. • Scroll to Edit. • Press 1: [A]. • Input...
https://education.ti.com/en/customer-support/knowledge-base/ti-83-84-plus-family/product-usage/34429