Education Technology

Knowledge Base Search

< Previous | 725 - 750 of 1765 results |  Next >

Solution 38017: Transferring an Operating System (OS) From Unit to Unit on the TI-89, TI-89 Titanium, TI-92 Plus, and Voyage 200.

...re unique and not cross compatible.Additional Note: Installing the OS will erase all data on the calculator.• Link two like units together.• On the receiving and the sending unit, press [2nd][VAR-LINK] to display the VAR-LINK screen.• On the receiving and the sending unit, press [F3] Link to disp...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/38017

Solution 35675: Connecting 60 Devices With USB 3.0 Ports Using TI-Nspire™ CX Docking Station.

... Why am I unable to connect all 60 devices on a USB 3.0 port using TI-Nspire CX Docking Station? Problem USB 2.0 and USB 3.0 ports are compatible and appear very similar. However, there are differences. USB 3.0 ports supports maximum of 30 devices including internal hubs. This means user can conn...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/35675

Solution 30571: Creating User Defined Units For Unit Conversion on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.

...ate unit cannot be found in the units menu a user may define a unit to store in the units menu. For example, to convert cubic feet into gallons or vice versa, it is known that 7.48051948 gallons is equal to one cubic foot. This value may be saved as _CUBFT in the units menu by following the step...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/30571

Solution 11840: Implicit Multiplication on the TI-89 Family, TI-92 Family, and Voyage™ 200.

...a reserved notation.The following are examples of how the implied multiplication is interpreted on the TI-89 family, TI-92 family, and Voyage 200 for certain expressions:1. Valid implied multiplication:• 2p is interpreted as 2 * p.• 4sin(46) is interpreted as 4 * sin(46).• 5(1+2) is interpreted a...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/general-information/11840

Solution 11837: Difference Between Complex Numbers on the TI-89 Family, TI-92 Family, or Voyage™ 200 Graphing Calculators.

...Base Search Are complex numbers handled differently on the TI-89 family, TI-92 family, and Voyage 200? The TI-92 and the TI-89 family/TI-92 Plus/Voyage 200 differ in the way polar form complex numbers are handled. The TI-92 accepts the form r*eiq and must be in radian mode. If entering ...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/general-information/11837

Solution 28630: Clearing and Deleting Lists using the Stats/List Editor Application on the TI-89 Family and Voyage™ 200.

.... There is also a way to delete all entries, including list name. To clear the entries within a list, but not deleting the list name: • Highlight the cell that holds the list name • Press the [CLEAR] key • Press the [Down] Arrow Notice that the list name is still available, however the list value...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/28630

Solution 11569: Algorithm Used for Finding the Determinant of a Square Matrix on the TI-81, TI-82, TI-83, TI-85, or TI-86.

...= [[ 2,-1,0][4,3,-3][8,-14,5]] which can also be expressed as: A = [[1,0,0][2,1,0][4,-2,1]]*[[2,-1,0][0,5,-3][0,0,-1]] Hence, L and U for this problem are: L = [[1,0,0][2,1,0][4,-2,1]] U = [[2,-1,0][0,5,-3][0,0,-1]] Once in this form, one may compute the det(A) as fol...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/11569

Solution 11401: Selecting Multiple Equations Under Different 'When' Headings in the ME*Pro® Application.

... In Beams and Columns of the Equations Section, equations for the slope of beam deflection are different depending on whether the deflection at distance x along the beam is calculated to the left side of the load (xa).  Since these conditions cannot simultaneously exist, ME*Pro restricts selectio...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/11401

Solution 10455: Equations Used to Create the Graphs on the TI-92 Plus Manual.

...raphs on the manual used the following equations and settings. MODE setting (Press [MODE])Graph...DIFF EQUATIONS Split Screen...LEFT-RIGHT Split 1 App...Y= Editor Split 2 App...Y= Editor Number of graphs...2 Graph 2...3D Split Screen Ratio...1:2 Left Graph Input the left side of the grap...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/10455

Solution 11731: Correcting the Error "ASAP or Exec string too long" Using the TI-89 Family, TI-92 Plus, and Voyage™ 200.

... correct the error ASAP or Exec string too long when running an assembly language program using the TI-89 family, TI-92 Plus, and Voyage 200? On Advanced Mathematics Software (AMS) 2.03 and above, the size limit of an assembly language program that can be executed is 24k. If an assembly language ...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/troubleshooting-messages-unexpected-results/11731

Solution 12041: Resolving the Error "Inconsistent Units" When Performing Temperature Conversions Using the TI-89 Family, TI-92 Family, and Voyage™ 200.

... Home | Other Graphing Calculator products Knowledge Base Knowledge Base Search Why do I receive an 'Inconsistent Units' error when performing temperature conversions on the TI-89 Family, TI-92 Family, Voyage 200? The 'Inconsistent Unit...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/troubleshooting-messages-unexpected-results/12041

Solution 23370: Solving Quadratic Equations on the TI-30X IIS/B and TI-34 II Explorer Plus™.

...] again for the result The screen should display -1. Please Note: To find the other value for the expression, use these set of instructions and replace [+] with the [-] (minus) key. Please see the TI-30X IIS/B and TI-34 II Explorer Plus guidebooks for additional information. Solution 23370: S...
https://education.ti.com/en/customer-support/knowledge-base/scientific-elem-calculators/product-usage/23370

Solution 11804: The Anti-Derivative of Sin(x)*Cos(x) Returns an Expression in Cos(x) Instead of Sin(x) on the TI-89 Family, TI-92 Plus and Voyage™ 200.

... Internally, the integrand is stored as cos(x)*sin(x). TI could have chosen to store the integrand as sin(x)*cos(x), but either ordering is equally acceptable. • Then the algorithm attempts to verify whether the integrand is of the form const*elementary_function(u(x))*u'(x). Here, the first fac...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/troubleshooting-messages-unexpected-results/11804

Solution 12685: Batteries For A Scientific Calculator.

... YES TI-32 2 - LR44 NONE NO TI-32 Explorer Plus NONE NONE YES TI-32 Solar NONE NONE YES...
https://education.ti.com/en/customer-support/knowledge-base/scientific-elem-calculators/general-information/12685

Solution 11845: Resolving the Error Message "Illegal Instruction" on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.

...: • Press and hold [2ND]. • Press and hold [LOCK] (the little hand). • While holding both, press [ON]. • Release all keys simultaneously. If this procedure does not restore the unit, remove a battery and press [ON] for 30 seconds. Replace the battery, turn on the unit, and adjust the contrast. ...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/troubleshooting-messages-unexpected-results/11845

Solution 12229: Differences Between the TI-10 and TI-15 Explorer™.

... audience than the TI-15 Explorer. Even though the calculators have many of the same features, some major differences were necessary to make it grade appropriate. The TI-10 has fewer and larger keys. The keys for fractions, the [0.001] thousandths key, p, square root,  [^] caret, and % have been ...
https://education.ti.com/en/customer-support/knowledge-base/scientific-elem-calculators/general-information/12229

Solution 12254: Converting Degrees Fahrenheit (°F) to Degrees Celsius (°C) on the TI-30X IIS/B.

...ease Note: The °C formula is as follows: °C=(°F-32)5/9 1) Press 32 [STO].  2) The screen will display A B C D E; use the arrow key to underline the appropriate letter.  3) Scroll to A and press [ENTER]. 4) Press 98.6 [-][2nd] [RCL]. (The screen will display A B C D E; move the right arrow and s...
https://education.ti.com/en/customer-support/knowledge-base/scientific-elem-calculators/product-usage/12254

Solution 10438: Performing Polar to Rectangular and Rectangular to Polar Conversions on the TI-85 and TI-86.

...e solution. The < symbol denotes the "angle" symbol on the calculator. To convert from rectangular to polar: 1) Input (5<53.13). Please Note: To access the < (angle) symbol, press [2nd] [,]. 2) Press [2nd] [CPLX] 3) Press [MORE] [F1] [ENTER] The screen will show (3.000..., 3.999...) as the s...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/troubleshooting-messages-unexpected-results/10438

Solution 12280: Calculating Standard Deviation on the TI-30X IIS/B, TI-30XS MultiView™ and TI-34 II Explorer Plus™.

...T], and then choose 1-VAR. 3) For the "DATA" option, choose the listname the data is stored in (L1, L2 or L3). For the "FRQ" option, choose "ONE" since this data does not include a frequency list. 4) Arrow down to "CALC" and press [ENTER]. Answers should be as follows: 3:Sx (Sample Standard De...
https://education.ti.com/en/customer-support/knowledge-base/scientific-elem-calculators/product-usage/12280

Solution 12281: Calculating the Log and Inverse Log of a Number Using the TI-34 II Explorer Plus™.

... the log and antilog of a number using the TI-34 II Explorer Plus. Example: Calculate the log of 1. 1) Press the [2nd] key, then the [LOG] key to access the LOG menu. 2) With the cursor under the 'LOG' function, press [=]. 3) Input [1]. Press [)] to close parentheses. 4) Press the [=] key. The...
https://education.ti.com/en/customer-support/knowledge-base/scientific-elem-calculators/product-usage/12281

Solution 12282: Changing the Angle Mode Setting on the TI-34 II Explorer Plus™.

...►] to highlight RAD. 3) Press [ENTER]. The calculator is now set to operate in the radian angle mode. To switch back to degrees, just use the same procedure but underline DEG instead. Resetting the calculator will also reset it back to factory default settings. To do this: 1) Press [2nd] [RESET]....
https://education.ti.com/en/customer-support/knowledge-base/scientific-elem-calculators/product-usage/12282

Solution 12295: Setting Scientific Notation Mode on the TI-34 II Explorer Plus™ and TI-34 MultiView™ Scientific Calculators.

...ion. The TI-30X IIS/B and TI-30XS/TI-30XB MultiView, which function in the same way as the TI-34 II Explorer Plus and TI-34 MultiView, are more advanced calculators that feature the option to display all results in scientific notation. Please see the TI-34 II Explorer Plus and TI-34 MultiView gu...
https://education.ti.com/en/customer-support/knowledge-base/scientific-elem-calculators/product-usage/12295

Solution 12320: Changing the Decimal Setting on the TI-30X IIB / TI-30X IIS and TI-34 II Explorer Plus™.

...ange the decimal format setting on the TI-30X IIB / TI-30X IIS and TI-34 II Explorer Plus: 1) Press [2nd] [Fix].2) Scroll to the number of decimal places to be displayed (0 - 9) and press the [=] key.3) To specify a floating-decimal format, scroll to "F" and press the [=] key. Please Note: "Fix" ...
https://education.ti.com/en/customer-support/knowledge-base/scientific-elem-calculators/product-usage/12320

Solution 12321: Difference Between [ (-) ] and [ - ] Keys on Two Line Elementary and Scientific Calculators.

...he [ (-) ] and the [ - ] key on TI's elementary and two line scientific calculators? There are two keys on TI's two line scientific calculators that appear to be similar. The [(-)] is the negate key, which is often mistakenly used as the subtraction key. The negation key converts a positive numb...
https://education.ti.com/en/customer-support/knowledge-base/scientific-elem-calculators/product-usage/12321

Solution 14484: Using the Inverse Function or Reciprocal on the TI-30X IIS/B.

... Home | Scientific, elementary & basic calculators Knowledge Base Knowledge Base Search How do I perform the inverse function on my TI-30X IIS/B? The inverse function is represented as x-1. The [x-1] key is located directly under the [SIN] key. P...
https://education.ti.com/en/customer-support/knowledge-base/scientific-elem-calculators/product-usage/14484