Education Technology

Solution 38017: Transferring an Operating System (OS) From Unit to Unit on the TI-89, TI-89 Titanium, TI-92 Plus, and Voyage 200.

How do I transfer an Operating System (OS) Unit to Unit on the TI-89, TI-89 Titanium, TI-92 Plus, and Voyage 200?

Please Note: You can only transfer from the same model of calculator to another as the OS files for the TI-89, TI-89 Titanium, TI-92 Plus, and Voyage 200 are unique and not cross compatible.


Additional Note: Installing the OS will erase all data on the calculator.

• Link two like units together.
• On the receiving and the sending unit, press [2nd][VAR-LINK] to display the VAR-LINK screen.
• On the receiving and the sending unit, press [F3] Link to display the menu options.
• On the receiving unit, select 5:Receive OS.
• A warning message displays press [ENTER] to proceed.
• On the sending unit, select 4:Send OS.
• A warning message displays. Press [ENTER] to start the transmission.

If you have questions about the information listed above, please contact TI-Cares for additional assistance.