Education Technology

Knowledge Base Search

< Previous | 325 - 350 of 1765 results |  Next >

Solution 34732: Archiving a Program Within Another Program Using the Command Line Archive PrgmName on the TI-83 Plus and TI-84 Plus Family of Graphing Calculators.

...rchived from within another program. Any instruction or expression that can be executed from the home screen can also be entered on a command line, except archiving another program. Please see the TI-83 Plus and TI-84 Plus Family guidebooks for additional information.Last updated: 7/03/2023 Solu...
https://education.ti.com/en/customer-support/knowledge-base/ti-83-84-plus-family/product-usage/34732

Solution 34843: Entering Complex Elements in a Matrix on the TI-83 Plus and TI-84 Plus Family of Graphing Calculators.

...84 Plus family of graphing calculators? The TI-83 Plus and TI-84 Plus family of graphing calculators do not allow the use of complex numbers in matrices.  If an imaginary or complex number is entered as a matrix element, a "DATA TYPE" error is returned. Please see the TI-83 Plus and TI-84 Plus F...
https://education.ti.com/en/customer-support/knowledge-base/ti-83-84-plus-family/product-usage/34843

Solution 34834: Typing Text Labels on Graph Screens on the TI-83 Plus and TI-84 Plus Family of Graphing Calculators.

...n writes text on graphs beginning at pixel (row, column), where 0£ row £57 and 0£ column £94. The function is located in the DRAW menu which can be accessed by pressing [2ND] [PRGM]. The syntax for the text() function is: text(row, column, text1, text2,…) Please refer to the example provided be...
https://education.ti.com/en/customer-support/knowledge-base/ti-83-84-plus-family/product-usage/34834

Solution 34797: Unit to Unit Transfer of an Operating System (OS) on the TI-84 Plus Family of Graphing Calculators.

... Plus Silver Edition TI-84 Plus Silver Edition to a TI-84 Plus Silver Edition TI-84 Plus C Silver Edition to a TI-84 Plus C Silver Edition TI-84 Plus CE to a TI-84 Plus CE • Connect the Mini A to Mini B USB cable to both calculators. • On the Sending calculator, press [2ND] [LINK]. • Scroll down ...
https://education.ti.com/en/customer-support/knowledge-base/ti-83-84-plus-family/product-usage/34797

Solution 34779: Correcting a Domain Error When Calculating a 1-Prop Z-Interval on the TI-83 Plus and TI-84 Plus Family of Graphing Calculators.

...r on the TI-83 Plus and TI-84 Plus family of graphing calculators? When calculating a 1-Prop Z Interval and the number of trials and the number of successes are given, it is important to input the trials in n and the number of successes in x. If this done incorrectly, the calculator will display ...
https://education.ti.com/en/customer-support/knowledge-base/ti-83-84-plus-family/product-usage/34779

Solution 34778: Creating a Box Plot on the TI-83 Plus and TI-84 Plus Family of Graphing Calculators.

...ailable in the menu) using the right arrow key and press [ENTER]. 4) Be sure that Xlist is L1. 5) Allow Freq to default to 1. Please Note: Color choice is only available on the TI-84 Plus CE and TI-84 Plus C Silver Edition. 7) Press [GRAPH] to see the Box Plot. Please Note:  Press [ZOOM], se...
https://education.ti.com/en/customer-support/knowledge-base/ti-83-84-plus-family/product-usage/34778

Solution 34772: Computing Net Present Value (NPV) and Internal Rate of Return (IRR) on the TI-83 Plus and TI-84 Plus Family of Graphing Calculators.

...r. • Press [5] [ENTER] [(-)] [4] [ENTER] [6]. • Press [►]. • Press [2] [ENTER] [3] [ENTER] [5] [ENTER]. Calculate NPV: • Press [2ND][QUIT]. • Press [APPS] [ENTER] [7]. • Press [7] [,] [(-)] [9] [,] [2ND] [L1] [2ND] [L2]. • Press [ENTER]. Calculate IRR: • Press [APPS] [ENTER] [8]. • Press [(-)] ...
https://education.ti.com/en/customer-support/knowledge-base/ti-83-84-plus-family/product-usage/34772

Solution 12290: Performing One-Variable Statistics on the TI-30X IIS/B, TI-30XS MultiView™ and TI-34 II Explorer Plus™ Calculators.

...e TI-30X IIS/B and TI-34 II Explorer Plus calculators. Data to use for this example: x = {71, 64, 55, 7,  98} To Solve: 1) Press [2ND] [DATA] to access the STAT menu. With the cursor (underline) below 1-VAR, press [ENTER]. The calculator is now in STAT mode. 2) Press [DATA] and begin to enter ...
https://education.ti.com/en/customer-support/knowledge-base/scientific-elem-calculators/product-usage/12290

Solution 11492: Editing And Transferring Programs Using TI Connect™ and TI Connect CE Software.

...ion of TI Connect software does not have a Program Editor.  However, TI Connect CE software can create and edit TI Basic programs. If you are using a TI-84 Plus Graphing Calculators family, please follow the instructions below:1) Download and install TI Connect CE software. 2) Launch TI Connect C...
https://education.ti.com/en/customer-support/knowledge-base/sofware-apps/product-usage/11492

Solution 11506: Transferring FLASH Applications (Apps) to a Graphing Calculator Using the TI Connect™ Software for Windows®.

...ow the steps below:1) Download and save the app file to the desktop or a folder on the desktop.2) Open the TI Connect software.3) Click on the TI Device Explorer icon. If the "Select TI Device" window appears, make sure the "Port", "Cable" and "Device" options are correct. Click the "Select" butt...
https://education.ti.com/en/customer-support/knowledge-base/sofware-apps/product-usage/11506

Solution 37039: What new features are included on the latest TI-Nspire™ and TI-Nspire CAS™ App for iPad® version 4.1?

... iPad® version 4.1? website Home | Computer Software, iPad and Chrome Apps Knowledge Base Knowledge Base Search What are the new features for the latest TI-Nspire™ and TI-Nspire™ CAS ...
https://education.ti.com/en/customer-support/knowledge-base/sofware-apps/general-information/37039

Solution 13401: Creating a DeviceInfo File Using TI Connect™ for Windows®.

...or Windows®. website Home | Computer Software, iPad and Chrome Apps Knowledge Base Knowledge Base Search How do I create a DeviceInfo file using TI Connect for Windows®? The TI Device...
https://education.ti.com/en/customer-support/knowledge-base/sofware-apps/product-usage/13401

Solution 11484: Creating a Program or Text File for a TI-89 Family, TI-92 Family, and Voyage™ 200 Using TI Connect™ Software for Windows®.

...or Windows®. website Home | Computer Software, iPad and Chrome Apps Knowledge Base Knowledge Base Search Can I create a program or text file using the TI Connect software for Windows?...
https://education.ti.com/en/customer-support/knowledge-base/sofware-apps/general-information/11484

Solution 14981: Choosing a Document Format When Using the TI NoteFolio™ Creator Software.

... as an application variable (AppVar) that can be sent to a TI calculator or classroom network. Please Note: Documents viewed on the TI-83 Plus Family/TI-84 Plus Family devices are limited to one note per document with a maximum document size of 20K. Documents viewed on the other TI calculators ca...
https://education.ti.com/en/customer-support/knowledge-base/sofware-apps/product-usage/14981

Solution 14960: TI CellSheet™ Converter for Macintosh® OS X.

...ntosh® OS X. website Home | Computer Software, iPad and Chrome Apps Knowledge Base Knowledge Base Search Has the TI CellSheet Converter been tested on Mac® OS X past 10.1? The TI Cel...
https://education.ti.com/en/customer-support/knowledge-base/sofware-apps/product-usage/14960

Solution 14881: Converting a CellSheet™ App AppVar Into a Microsoft® Excel Spreadsheet.

...llSheet Converter software. The TI CellSheet Converter software copies the device file to a temporary directory on the computer and displays the path for the converted file. The device file is selected for conversion by default, that is, it has a checkmark beside the path and file name. • Close T...
https://education.ti.com/en/customer-support/knowledge-base/sofware-apps/product-usage/14881

Solution 40361: Student Data Privacy Policy for TI Software and Apps

... and are not generally considered to be harmful if disclosed. TI respects student data privacy and protects this directory information in accordance with TI’s Student Data Privacy Policy education.ti.com/en/product-resources/datapolicy. This policy describes TI practices for handling stud...
https://education.ti.com/en/customer-support/knowledge-base/sofware-apps/general-information/40361

Solution 13403: Removing the TI Tools Menu from Microsoft® Office 2003 Applications.

... How can I remove the TI Tools menu from Microsoft® Office Word 2003? Installing the NotoFolio™ Creator software also installs a TI Tools menu for Microsoft® Office applications, specifically Microsoft® Office 2003. To remove the TI Tools menu:• Close all Microsoft® Office applications.• G...
https://education.ti.com/en/customer-support/knowledge-base/sofware-apps/product-usage/13403

Solution 15589: Creating a Multiple-Choice with Levels StudyCards™ Stack Using the StudyCards Creator Software.

...ing the StudyCards Creator software, follow the steps below:• Open the StudyCards Creator software.• Select the device type (TI-73, TI-83 Plus Family/TI-84 Plus Family, TI-89 Family, TI-92 Plus, Voyage 200).• Select Multiple-Choice with Levels as the stack type.• Click OK. The Multiple-Choice wit...
https://education.ti.com/en/customer-support/knowledge-base/sofware-apps/product-usage/15589

Solution 11733: Creating Groups Using the TI Connect™ Software for Windows®.

...e of device connected to the PC. Additional Note: These steps apply to the following calculators models: TI-73 Explorer™ TI-83 and TI-83 Plus Family TI-84 Plus C Silver Edition TI-84 Plus Silver Edition TI-84 Plus TI-86 TI-89/TI-89 Titanium TI-92 and TI-92 Plus Voyage™ 200 Solution 11733: Creat...
https://education.ti.com/en/customer-support/knowledge-base/sofware-apps/product-usage/11733

Solution 33131:Resolving the Error "Can't Be Opened Because It Is From An Unidentified Developer" or ".pkg can't be Opened Because Apple Cannot Check for Malicious Software." When Installing Texas Instruments Software Products Using a Mac.

...ttempting to install. 2) Hold [Ctrl] then [Click] the TexasInstrumentsSoftware.pkg and choose [Open] from the menu that appears. 3) The warning you received previously will still display but you will be given the option to [Open] the pkg and continue with the install. Please Note: If you are u...
https://education.ti.com/en/customer-support/knowledge-base/sofware-apps/troubleshooting-messages-unexpected-results/33131

Solution 40257: TI-SmartView CE and TI Connect CE Application Flagged as Unsafe by Microsoft Defender SmartScreen

...because Windows Defender is flagging our installer as unsafe. This warning may stop appearing after further data is collected by Microsoft. Further information can be found at the Microsoft Article below:    https://docs.microsoft.com/en-us/windows/security/threat-protection/microsoft-defender-sm...
https://education.ti.com/en/customer-support/knowledge-base/sofware-apps/troubleshooting-messages-unexpected-results/40257

Solution 38675: TI-Smartview CE Save Emulator State is Greyed-Out.

... Why is TI-Smartview CE "Save Emulator State" Greyed-Out? TI-Smartview CE "Save Emulator State will be Greyed-Out when using the emulator modes "TI-84 Plus" or "TI-84 Plus C". The TI-Smartview CE "Save Emulator State" option is only available when using the emulator mode "TI-84 Plus CE", to ...
https://education.ti.com/en/customer-support/knowledge-base/sofware-apps/troubleshooting-messages-unexpected-results/38675

Solution 38155: TI-Nspire™ Apps for iPad® Closes Unexpectedly when using a Calculator page after updating.

...n using a Calculator page after updating because of an issue identified by our development team.To workaround this issue create a new document and proceed to use the new document the issue will not occur again.If you have questions about the information listed above, please contact TI-Cares for a...
https://education.ti.com/en/customer-support/knowledge-base/sofware-apps/troubleshooting-messages-unexpected-results/38155

Solution 40456: Resolving Errors ET100, ET101, ET102, ET103, ET104, ET106, ET199, V201, V202, V203, V204, V205, V206, V207, V299 and V999 for Account-Based Licenses.

...d Licenses. website Home | Computer Software, iPad and Chrome Apps Knowledge Base Knowledge Base Search How to resolve errors ET100, ET101, ET102, ET103, ET104, ET106, ET199, V201, V...
https://education.ti.com/en/customer-support/knowledge-base/sofware-apps/troubleshooting-messages-unexpected-results/40456