Education Technology

Knowledge Base Search

< Previous | 1025 - 1050 of 1414 results |  Next >

Solution 12061: Calculating Logs on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.

...age 200 graphing calculators? The Logarithm (log) function on the TI-89 family, TI-92 family, and Voyage 200 is located in the [CATALOG] menu. To access this function: • Press [CATALOG] [L]. • Scroll to log( , press [ENTER]. • Input the value. • Close the parentheses and pr...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/12061

Solution 12059: Implicit Partial Differentiation on the TI-89 Family, TI-92 Family, or Voyage™ 200 Graphing Calculators.

...nd TI-89 Titanium operating system contain a impdif ( command. This command should be used when computing a implicit partial differentiation. To access the command, press [F3] [Up Arrow] [Enter] on the homescreen. For example, to solve the equation x^2+y^2=0, enter impdif(x^2+y^2=0, x, y) and...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/12059

Solution 12069: Storing a Value to a Matrix Element on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.

...3) To create the matrix above, the Type: will be Matrix, the Variable: name is A, and the row and column dimensions are both 2.  4)Press [ENTER] twice.  5) Input the values that are above in the Data/Matrix Editor in sequence from left to right. If "A" is a 2x2 matrix, then to store the value o...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/12069

Solution 12046: Calculating Two-Variable Statistics on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.

...PPS] use the arrows to select [Data/Matrix Editor] and press [ENTER]. 2) Choose [3: New] then press [Enter]. 3) Press [Down Arrow] [Down Arrow] to place the cursor in the variable box then enter a variable name for example: datab. 4) Press [ENTER] [ENTER] to open the editor. 5) Enter the x value...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/12046

Solution 12067: Population Standard Deviation on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.

... the denominator. The TI-89 family, TI-92 family, and Voyage 200 graphing calculators use the sample standard deviation Sx when calculating the variance (Sx2).Once the statistical analysis has been performed, to find the population standard deviation, input sx on the home screen. To access this v...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/12067

Solution 11806: Creating and Evaluating User-Defined Functions on the TI-89 Family, TI-92 Family and Voyage™ 200.

...ents for subsequent functions or programs. In the argument list, be sure to use the same arguments that are used in the definition. Arguments are placeholders that represent whatever values passed to the function. Functions can be created using one of the following methods: 1. Using the [STO->...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/11806

Solution 12066: Performing Number Base Conversions on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.

...The TI-92 does not have the base conversion function built into it but the function can be added through a function. Please see page 344 of the TI-92 Plus guidebook. Please see the TI-89 family, TI-92 family and Voyage 200 guidebooks for additional information. Solution 12066: Performing Number...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/12066

Solution 12042: Algorithm for Summation on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.

...o use and compute summations using the TI-89 family, TI-92 family, and Voyage 200 graphing calculators. The syntax for the å ( function, which is accessed by pressing [2nd] [MATH] [B] [4], is as follows: å(expression, variable, lower limit, upper limit) Example: To find the sum of the seque...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/12042

Solution 12136: Factoring an Expression on the TI-89 Family and Voyage 200 Graphing Calculators.

...y, the TI-92 Family and the Voyage 200. The proper syntax for the factor() command is factor(expression)For Example: factor(x^2-6x+5) Some good practices when factoring expressions:1) Delete all one-character variables by pressing F6:Clean Up ([2nd] [F1] on the TI-89 family), selecting 1:Clear a-...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/12136

Solution 11769: Graphing Coordinates Using the TI-89 Titanium and Voyage™ 200 Graphing Calculators.

...New and press [ENTER]. Select Data for the Type and select main for the Folder. Next to Variable, type in a name for the data list (the name cannot exceed 8 characters) and press [ENTER] twice.3) Under c1, type in all the X-values (2,3,4). Under c2, type in all the Y-values (5,6,7).4) Press the [...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/11769

Solution 11869: Performing Unit Conversions On The TI-89 Family,TI-92 Family, and Voyage™ 200 Graphing Calculators.

...o another in the same category, including user-defined units. For example, to convert 4 light years to kilometers: • Enter 4 • Press [2nd][3] to access the UNITS menu (On Voyage 200 press [♦][P]) • In the Length menu, select _ltyr, • Press [2nd][MODE] to select the convert icon (on the V...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/11869

Solution 11755: Finding the Row Echelon Form of a Matrix Using a TI-89 Family, TI-92 Family, or Voyage™ 200 Graphing Calculator.

...). 2) Press [►] [2] [▼] [▼] [B] [▼]. 3) Press [ALPHA]. Users with a TI-92 family or Voyage 200 graphing calculator may omit this step or any reference to pressing [2ND] [LOCK]. 4) Press [3] [▼] [3] [ENTER]. 5) Press [ENTER] [5] [ENTER] [(-)] [6] [ENTER] [9] [ENTER]. 6) Press [4] [ENTER] [7] [E...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/11755

Solution 12133: Entering a List on the Home Screen using the TI-89 Family, TI-92 Family, or Voyage™ 200 Graphing Calculators.

...t on the home screen of a TI-89 Family, TI-92 Family or Voyage 200. Example: Create a list, called "test" which contains the values {1,2,3,4}. 1) Access the home screen by pressing the [HOME] key on the TI-89 and TI-89 Titanium, [GREEN DIAMOND] [HOME] on the TI-92 family, or [GREEN DIAMOND] [CA...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/12133

Solution 11863: The factor() Function Algorithm on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.

... TI-92 family, and the Voyage 200? The factor() function returns the rational number factored into primes and a residual having prime factors that exceed 65521. The methods include the well-known factorizations of binomials and quadratics, together with methods described by Geddes, Czapor and ...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/11863

Solution 11853: The Algorithm for cFactor() Function on the TI-89 Family, TI-92 Family, and Voyage 200™ Graphing Calculators.

...family, TI-92 family, and Voyage 200 graphing calculators? The algorithm for cFactor() function is the same as the Algorithm For Factor() Function except the domain is temporarily set to complex so that complex factors are sought and not rejected. Please see the TI-89 family, TI-92 family, and V...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/11853

Solution 12124: Computing the Average Rate of Change of an Expression on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.

...s found under [CATALOG].The syntax of the avgRC function is avgRC(expression, var,[h]) h is optional.The avgRC() function returns the forward difference quotient of the expression. The expression can be a user-defined function. h is the step value and if h is omitted, it defaults to 0.001.Example...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/12124

Solution 11789: Solving Quadratic Equations using the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.

... Press [1] [0] [=] [0]. 5) Press [,] [X] [)]. 6) Press [ENTER]. In addition, the Polynomial Root Finder App is available for the TI-89 family, TI-92 Plus, and Voyage 200. Please see the TI-89 family, TI-92 family and Voyage 200 guidebooks for additional information. Solution 11789: Solving Qua...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/11789

Solution 10586: Temperature Unit R on the TI-85, TI-86, TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.

... R is used to denote Rankine, which is an absolute temperature measurement in English units. Rankine is to Fahrenheit as Kelvin is to Celsius. 1 Rankine= -458.67° Fahrenheit Please see the appropriate model of graphing calculator guidebooks for additional information. Solution ...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/10586

Solution 10349: Calculation Method Used by the Polynomial Root Finder on the TI-85 and TI-86.

...lled a "companion matrix". Basically, the coefficients appear across a row or column (there are variations) and the rest of the matrix is all zeros except for a pattern of ones just off the main diagonal. The property of this matrix is that the characteristic polynomial of the matrix will be the...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/10349

Solution 10583: Inverse or Reciprocal Function on the TI-86.

... Knowledge Base Search How do I use the inverse function on the TI-86? The inverse function, x-1, on the TI-86 is accessed by pressing [2nd] [EE]. The inverse function will take the inverse of a number, list, function, or a square matrix. To take the inverse of ...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/10583

Solution 12115: Calculating the Transpose of a Matrix using the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.

...) To create the matrix above, the Type: will be Matrix, the Variable: name is A, and the row and column dimensions are both 2.  4) Press [ENTER] twice.  5) Input the values that are above in the Data/Matrix Editor in sequence from left to right. To find the transpose: 1) From the Home screen 2)...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/12115

Solution 10580: Finding the Area Below a Function Using a TI-86.

... numerical approximation for a definite integral, uses the following syntax: FnInt(expression, variable name, lower limit, upper limit) NOTE: To access this function, press [2nd] [CALC] [F5]. Example: What is the area under the function y = 2 - 2x between -2 and 1? • Press [2nd] [CALC] [F5]....
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/10580

Solution 10350: Finding the Determinant and Inverse of a Matrix on the TI-85 or TI-86.

... • Select A • Press [ENTER] To find the inverse of a square matrix, type in the name, then press [2nd] [EE], and then press [ENTER]. If the matrices determinant equals 0 an error message of "ERROR 02 DIV BY ZERO" will be returned. Please see the TI-85 and TI-86 guidebooks for additional info...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/10350

Solution 10352: Inputting Complex Numbers on the TI-85 or TI-86 Graphing Calculators.

...complex number in polar form is to separate the magnitude and angle using the angle symbol. The syntax is: (magnitude < angle). The angle symbol is accessed by pressing [2nd] [,]. Please refer to the examples provided below:Please Note: To activate complex mode press [2nd][CPLX].(3+7i) would be i...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/10352

Solution 10578: Degree, Minutes, Seconds (DMS) Conversions with the TI-82.

...quote after each value. For example, to convert 15 degrees, 12 minutes and 8 seconds to decimal degrees, input 15'12'8' and press [ENTER]. The ' is accessed by pressing [2nd] [ANGLE] [2]. To convert a number that is written in decimal degrees to DMS, follow the example below: Convert 12.2525 to...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/10578