Education Technology

Knowledge Base Search

< Previous | 1375 - 1400 of 1765 results |  Next >

Solution 12106: Verifying a Symbolic Result on the TI-89 Family, TI-92 Family, or Voyage™ 200 Graphing Calculators.

...d and the result from the calculator. • Set each function equal to one another to see if the calculator returns a "true" statement.  • Substitute appropriate random values for some or all of the variables in each of the two expressions. Please see the TI-89 family, TI-92 family and Voyage 200...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/12106

Solution 10376: Compatibility of the DataMate Program and the TI-82 Graphing Calculator.

...m? The TI-82 can run parts of the DataMate program for the CBL 2. It is recommended that programs such as ChemBio, Physics, etc., are used instead since the DataMate program requires more memory than the TI-82 can use to run the program optimally.Please see the TI-82 guidebook for additional info...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/general-information/10376

Solution 12102: Printing the History Area on TI-89 Family, TI-92 Family, or Voyage™ 200 Graphing Calculators.

... object, follow these steps: • From the Home Screen, press [F1]. • Select Save Copy As.... • Give the text file a name and press [ENTER].    Once the data has been saved, the file can be opened in the text editor of the graphing calculator or sent to the computer for printing. Please see ...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/12102

Solution 30531: Finding the Inverse of a Function on the TI-89 Family, TI-92 Family and Voyage™ 200 Graphing Calculators.

... and Voyage 200 calculator? For example, if you need to find the inverse of f(x)=5/x+10 follow the steps listed below. 1) On a sheet of paper, replace x with y, and replace f(x) with x 2) Your equation should now be x=5/y+10 3) Solve for y using your calculator by pressing: [F2] [ENTER] [x] [=]...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/30531

Solution 11856: Definition of the ClrHome Function on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.

...rrent entry line. For functions such as solve() that return arbitrary constants or integers (@n1, @n2, etc...), ClrHome resets the suffix to 1. To access and execute the ClrHome function using the TI-89 family calculator, press [HOME] [CATALOG] [)], scroll down to ClrHome and press [ENTER] [ENTE...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/general-information/11856

Solution 29130: Calculating and Graphing Quadratic Regressions Using the TI-73 Family Calculator.

...he regression equation to the Y= Editor so that the function can be graphed. The calculator should display values for the variables a, b, and c. Since the function for the quadratic regression is ax^2 + bx + c, the solution can be interpreted as: -1.25x^2 + 13.75x - 20.75 Please Note: To displa...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/29130

Solution 10421: Creating and Using Strings on the TI-86.

...oducts Knowledge Base Knowledge Base Search How do I create and use strings on the TI-86? A string is a sequence of characters that are enclosed within quotation marks. Strings define characters to be displayed in a program and accept input from the keyboar...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/10421

Solution 11130: Availability of A Hard Copy Voyage™ 200 Guidebook.

...ard copy of the Voyage 200 guidebook available? The Voyage 200 does not come with a full printed guidebook. The Voyage 200 is an upgrade to the TI-92 Plus. The functions and commands for the TI-92 Plus are found on the Voyage 200. The hard copy TI-89/TI-92 Plus comprehensive guidebook can be used...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/general-information/11130

Solution 10577: Converting Units of Measure on the TI-85 and TI-86.

...dge Base Search How do I convert units of measure on the TI-85 and TI-86? To convert units of measure on the TI-85 and TI-86, follow this procedure:Enter the value to be converted. Press [2nd] and [CONV] to display the CONV menu. Press the corresponding F key for the category of the unit...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/10577

Solution 10576: Converting Binary Numbers Into Decimals on the TI-85 or TI-86 TI Graphing Calculators.

...ducts Knowledge Base Knowledge Base Search How can a binary number be converted into a decimal on a TI-86? Once the mode on theTI-85 or TI-86 has been changed to degree, a binary number can then be converted into a decimal. To change the mode, follow the ...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/10576

Solution 13886: Calculating Implicit Derivatives on the TI-89 Titanium and Voyage™ 200 with OS v3.10. or Higher.

...se of OS v3.10, the impDif() function has now been added to the operating system of the TI-89 Titanium and Voyage 200. The impDif() function can be accessed by following the steps provided below. 1) From the HOME screen, access the Calc menu by pressing [F3] 2) Select D:impDif( -or- 1) From the...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/13886

Solution 13882: Calculating Logs With Different Bases on the TI-89 Titanium and Voyage™ 200 with OS v3.10.

...o bring up the log command.  2) Input [1][0][,][2][)] and press [ENTER] for the result of 3.32193 to be displayed. Please Note: The calculator Exact/Approx mode should be set to APPROXIMATE. Please see the TI-89 Titanium and Voyage 200 guidebooks for additional information. Solution 13882: C...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/13882

Solution 15909: Finding the Two's Complement of a Binary Number Using the TI-36X Solar Scientific Calculator.

...nary number using the TI-36X Solar scientific calculator? Two's complement is an operation of negation (converting positive to negative numbers or vice versa) in computers. In an n-bit binary number, the most significant bit is usually the 2^(n-1)'s place. But in the two's complement representa...
https://education.ti.com/en/customer-support/knowledge-base/scientific-elem-calculators/product-usage/15909

Solution 15629: Graphing Functions with Fractional Powers on Texas Instruments Products Where X < 0.

...er, as mentioned above, the principal branch of x^y is not real for x0 because the derivative is 1/(3x^(2/3)), but der1(x^(2/3),x) plots for all x (except x=0) even though x^(2/3) doesn't plot for x<0, because the derivative is 2/(3x^(1/3)). Solution 15629: Graphing Functions with Fractional Pow...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/general-information/15629

Solution 33731: Calculating Two-Variable Statistics on the TI-36X Pro.

...follow the steps below: • Press [data]. • Under L1, input [1] [0] [enter] [2] [5] [enter] [3] [0] [enter] [4] [0] [enter]. • Press the right arrow once and input [5] [enter] [3] [0] [enter] [5] [0] [enter] [7] [0] [enter]. To calculate the statistical variables, please follow the steps below: ...
https://education.ti.com/en/customer-support/knowledge-base/scientific-elem-calculators/product-usage/33731

Solution 33912: Solving a System of Linear Equations Using the TI-36X Pro.

...near equations using the TI-36X Pro. The options are 2x2 LIN EQUs and 3x3 LIN SYSTEM. The 2x2 option shows x and y on the screen and also you use the plus or the minus key. The 3x3 option will only show zeros where your entry would go and you may use the negative or minus key. For Example:3x + 3y...
https://education.ti.com/en/customer-support/knowledge-base/scientific-elem-calculators/product-usage/33912

Solution 12710: Entering Numbers in Scientific Notation on a Scientific Calculator.

...ase Note: The TI-30XS MultiView™ scientific calculators do not have an [EE] key. Instead they have a shortcut key, [x10n] which can be used in its place.Please see the guidebooks for additional information. Solution 12710: Entering Numbers in Scientific Notation on a Scientific Calculator. ...
https://education.ti.com/en/customer-support/knowledge-base/scientific-elem-calculators/product-usage/12710

Solution 34033: Calculating Factorials on the TI-36X Pro.

...e example below will demonstrate how to calculate factorials on the TI-36X Pro. Example: What is the factorial of 10? • Press [1] [0] [! nCr nPr] once to show ! then press [enter]. The answer will show 3628800. Please see the TI-36X Pro guidebook for additional information. Solution 34033: ...
https://education.ti.com/en/customer-support/knowledge-base/scientific-elem-calculators/product-usage/34033

Solution 34034: Calculating the Inverse of a Matrix Using the TI-36X Pro.

...e the Inverse of Matrix A: Solution: To enter the matrix: • Press [2nd] [matrix] • Use the [right arrow key] and scroll to EDIT • Press [enter] to access matrix A • Input the dimensions by selecting 2 for ROWS and 2 for COLUMNS • Scroll to OK and press [enter] • Input the matrix entries, pressi...
https://education.ti.com/en/customer-support/knowledge-base/scientific-elem-calculators/product-usage/34034

Solution 15402: Numeric Notation Modes on the TI-30X IIS/B, TI-30XS MultiView™ and TI-34 MultiView™ Scientific Calculators.

...e TI-30X IIS/B, TI-30XS MultiView, and TI-34 MultiView. The TI-30X IIS has (3) numeric notation modes - FLO, SCI, and ENG. The mode settings can be accessed by pressing [2nd] [SCI/ENG]. The TI-30XS MultiView has (3) numeric notation modes - NORM, SCI, and ENG. The mode settings can be accessed by...
https://education.ti.com/en/customer-support/knowledge-base/scientific-elem-calculators/product-usage/15402

Solution 11851: Summation or Sum() Function Algorithm on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.

... Home | Other Graphing Calculator products Knowledge Base Knowledge Base Search What is the algorithm for the Summation or sum() function? The sum() function uses iterated addition for numeric limits. Other sums are determined from formulas given i...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/general-information/11851

Solution 34293: Computing Binomialcdf on the TI-36X Pro.

...36X Pro? Binomialcdf computes a cumulative probability at x for the discrete binomial distribution with the specified numtrials and probability of success (p) on each trial. x can be nonnegative integer and can be entered with options of SINGLE, LIST or ALL (a list of cumulative probabilities is ...
https://education.ti.com/en/customer-support/knowledge-base/scientific-elem-calculators/product-usage/34293

Solution 40477: Troubleshooting a TI-30XS MultiView™ and TI-34 MultiView Scientific Calculator that will not turn on.

... is available at the bottom of the calculator and if so, use a pen to press this button.  • If the screen stays blank the battery may need to be replaced, please visit Solution 40317 for battery replacement information. If you require additional assistance please contact TI-Cares. Last updated: ...
https://education.ti.com/en/customer-support/knowledge-base/scientific-elem-calculators/troubleshooting-messages-unexpected-results/40477

Solution 12325: Troubleshooting a Two-line Display Scientific Calculator that Will Not Turn On.

...ill fail to power on. Follow the steps below to reset the calculator: 1) Hold down [CLEAR] and [ON] key at the same time. 2) Release both keys. 3) Once the keys have been released, the calculator should display a blinking cursor. Please Note: If the blinking cursor is not displayed, press the [O...
https://education.ti.com/en/customer-support/knowledge-base/scientific-elem-calculators/troubleshooting-messages-unexpected-results/12325

Solution 35012: Calculating nth Roots Using the TI-36X Pro.

... Home | Scientific, elementary & basic calculators Knowledge Base Knowledge Base Search How do I perform nth root computations using the TI-36X Pro?  The example below will demonstrate how to perform nth root computations on the TI-36X Pro.Example...
https://education.ti.com/en/customer-support/knowledge-base/scientific-elem-calculators/product-usage/35012