Knowledge Base Search
Solution 10583: Inverse or Reciprocal Function on the TI-86.
... Knowledge Base Search How do I use the inverse function on the TI-86? The inverse function, x-1, on the TI-86 is accessed by pressing [2nd] [EE]. The inverse function will take the inverse of a number, list, function, or a square matrix. To take the inverse of ...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/10583
Solution 10350: Finding the Determinant and Inverse of a Matrix on the TI-85 or TI-86.
... • Select A • Press [ENTER] To find the inverse of a square matrix, type in the name, then press [2nd] [EE], and then press [ENTER]. If the matrices determinant equals 0 an error message of "ERROR 02 DIV BY ZERO" will be returned. Please see the TI-85 and TI-86 guidebooks for additional info...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/10350
Solution 12100: Calculating Inverse Logarithms or Antilogs on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.
...the TI-89 family, TI-92 family or Voyage 200 graphing calculators? The inverse log of a number N is equal to 10^N. 10^ can be entered manually or accessed through the CATALOG menu. Example: To calculate the inverse log of 1.25, enter 10^1.25, which returns 17.7828. Please see the TI-89 fami...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/12100
Solution 12062: Calculating Median-Median Regression Using the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.
... family, and Voyage 200. Data for this example: X values = {5, 9, 20, 25, 30, 35, 41} Y values = {4, 31, 42, 39, 20, 55, 73} Solution: 1) Press [APPS] [6] [3] (If the Apps Desktop is on, press [APPS], select "Data/Matrix Editor", and press [3]). 2) Scroll down to "3:New" and press [ENTER]. ...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/12062
Solution 10397: Calculating One-variable Statistics on the TI-85.
...ow do I calculate one-variable statistics on the TI-85? The example below will demonstrate how to calculate one-variable statistics on the TI-85.Data for this example:x values={5, 9, 7, 4, 6, 250, 35, 100, 84} Clear the screen then press [STAT] [F2] [F1] [ENTER] [ENTER] The cursor will disp...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/10397
Solution 10373: Calculating One-Variable Statistics on the TI-82.
...ow do I calculate one-variable statistics on the TI-82? The example below will demonstrate how to calculate one-variable statistics on the TI-82.Data for this example:x values={5, 9, 7, 4, 6, 250, 35, 100, 84}• Press [STAT] [ENTER] to enter the statistics list editor.• Enter the numbers into the ...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/10373
Solution 22171: Pausing a Program on a TI-89 Family, TI-92 Family and Voyage™ 200 Graphing Calculator so Entire Results May Be Viewed.
...ase Search How can I pause a program so that I may view the entire result? If a program requires more information than can be displayed at once, users may add a Pause command in the program to pause it until they are ready to continue. This is especially useful when displaying long lists...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/22171
Solution 11505: Sending Files from a TI-82 or TI-85 to a Macintosh® with the TI-GRAPH LINK 2 or the TI Connect™ Software.
...85 to a Macintosh® with the TI-GRAPH LINK 2 or the TI Connect software? When sending files to a Macintosh® computer from a TI-82 or a TI-85, it is necessary to access the LINK menu on the calculator, select the variables to transmit, and select TRANSMIT on the TI-82 and SEND on the TI-85. Note: ...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/11505
Solution 10371: Calculating and Graphing a Linear Regression on the TI-82.
...] [1].2) Press [ENTER] to turn on the stat plot.3) Be sure that xlist is L1 and ylist is L2 4.4) Press [GRAPH] to display the data. Note: it may be necessary to change the window view.Graph the linear regression:1) Press [Y=].2) Press [VARS] [5] scroll to EQ press [7].3) Press [GRAPH]Please see t...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/10371
Solution 11595: Displaying of a Numeric Answer Instead of a Symbolic Answer when Using the Integration Function on the TI-89 Family, TI-92 Family, or Voyage™ 200 Graphing Calculators.
...tion. Variables can be deleted by pressing [F6][ENTER] from the home screen or by using the DelVar command. The calculator resorted to a numerical approach to find the solution for the problem. This could happen when the problem being solved is too 'complex' for the symbolic algorithm to sol...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/11595
Solution 11775: Inserting Comments in a TI Basic Program on the TI-89 Family, TI-92 Family, and Voyage™ 200.
... Knowledge Base Search Can I insert comments in TI Basic program on the TI-89 family, TI-92 family, and Voyage 200? Text placed after the © symbol indicates a program comment. Any information to the right of the © symbol will not be executed when the program runs.The © s...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/11775
Solution 10416: Calculating the Derivative of a Function Using the TI-85 or TI-86.
... not give the symbolic answer of 2x+2. Instead, the graphing calculator substitutes 2 (for x) into the answer (2x+2) and evaluates the function, hence the answer of 6.Please see the TI-85 and TI-86 guidebooks for additional information. Solution 10416: Calculating the Derivative of a Function ...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/10416
Solution 11770: Graphing Polar Rose Functions on the TI-89 Family, TI-92 Family and Voyage™ 200 Graphing Calculators.
...mily and Voyage 200. Example: r=8*sin(2.5q) 1) Press [MODE], change the Graph mode to Polar, change the Angle mode to Radian, and press [ENTER] twice to save the new graph and angle mode settings. 2) Now press the [Diamond Key] and [F1] to enter the equation into the graphing editor. 3) Pres...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/11770
Solution 18689: Calculating the gcd() (Greatest Common Divisor) on the TI-73 Family Graphing Calculators.
...-list, the non-list is paired with each element of the list, and a list is returned. Note: This is function is frequently used with fractions to reduce them to lowest terms on the TI-73 family. The syntax is as follows: gcd(valueA,valueB) Examples: • Find the greatest common divisor fo...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/18689
Solution 11712: Calculating Standard Deviation on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.
... 5, -6, 3, -2} • From the HOME screen, press [2ND] [MATH] • Select 6:Statistics and 6:stdDev • Input the data {1, 2, 5, -6, 3, -2}, and press [)] • Once the screen displays stdDev({1, 2, 5, -6, 3, -2}) press [ENTER] to calculate the result of 3.937 or square-root (62)/2 Ex. Calculate the Standar...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/11712
Solution 11763: Graphing a Differential Equation on the TI-89 Family, TI-92 Family and Voyage™ 200 Graphing Calculators.
...turn to the main screen. 5) Press [♦][F1] (On the TI-92 family and Voyage 200 press [♦][W]) 6) Enter y1'= 2y1*cos(t). Please Note: That the y is replaced with y1. This is because y' is itself replaced with y1'. 7) Press [F1][9] to access the Format menu. 8) Make sure that the setting Axes ...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/11763
Solution 18649: Finding the Length of a Vector Using the TI-89 Family, TI-92 Family and Voyage™ 200 Graphing Calculators.
...itd default mode settings. To do this press [2nd] followed by [6]. Then press [F1], choose Default and press [ENTER] until the "Defaults Set" message appears. 1) On the Home screen, press [CATALOG] [6] and scroll down to norm(). 2) Press [ENTER]. On the Voyage 200 and TI-92 family press [2nd] [C...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/18649
Solution 10383: Shading Above or Below a Function on the TI-82.
...shade above or below a function on the TI-82? Using the shade command, the TI-82 can shade a specific area of the graphing window. This function is accessed by pressing [2nd] [DRAW] [7]. The first two arguments in the shade command define the area that will be shaded. The first is the lower bound...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/10383
Solution 11751: Finding Critical Points Using the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.
...) Press [F2] and select solve( and enter solve(3x^2+2x-5=0,x) This will solve for the unknown value, x, and return the following :x=1 or x= -5/3. Since there are two answers for the following function, there will be two sets of critical points on this function. To solve for the additional points...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/11751
Solution 11737: Deleting Programs on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.
...delete a program from a TI-89 family, TI-92 family, and Voyage 200, follow the instructions listed below.• From the Home screen, press [2nd] [-] to access the VAR-LINK menu.• Use the arrow keys to scroll to the name of the program to delete.• Press [F1] to select the Manage menu.• Select 1:Delete...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/11737
Solution 27750: Finding the Intersection of Two Functions on the TI-73 Explorer™ Graphing Calculator.
...tore the value for the X intersection point to the variable A so you can recall it later. 7) Press [GRAPH] to graph the functions. 8) Press [TRACE] [2nd] [TEXT] [Enter] [↓] [↓] [↓] [↓] [Enter] [Enter] this will display both your X intersection point and your Y intersection point. For addit...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/27750
Solution 10354: Running TI-85 Programs on a TI-86.
Solution 10354: Running TI-85 Programs on a TI-86. Solution 10354: Running TI-85 Programs on a TI-86. global Solution 10354: Running TI-85 Programs on a TI-86. website Home | Other Graphing Calculator pr...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/10354
Solution 11708: Calculating Natural Logarithm on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.
...xamples will demonstrate how to compute natural logs on the TI-89 Family, TI-92 Family, and Voyage 200 graphing calculators:Note: On the TI-92, TI-92 Plus, and Voyage 200, use the [LN] key. For the TI-89 and TI-89 Titanium, use the [2nd] [LN] keys.Natural log of 100. (4.6051.......)• Press the [L...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/11708
Solution 30350: Using the Two-Graph Mode on the TI-89 Family and Voyage™ 200 Graphing Calculators.
... etc. • Graph screens. Note: If both sides use the same graphing mode, each side can select different functions from the Y= Editor. Non-graph-related applications (Home screen, Data/Matrix Editor,etc) are shared and can be displayed on only one side at a time. Setting the Mode Several mode sett...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/30350
Solution 14564: Turning Off the Axes on the TI-89 Family and Voyage™ 200 Calculators.
...n off the axes on my Voyage 200 or TI-89 family calculator? To turn off the axes on the TI-89 family calculators: • Press [GREEN DIAMOND] [F1] to access the Y= Editor.• Press [F1] to access the "Tools" menu.• Press [9] for Format.• Scroll down and highlight "ON" to the right of "Axes". Press ...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/14564