Education Technology

Solution 22171: Pausing a Program on a TI-89 Family, TI-92 Family and Voyage™ 200 Graphing Calculator so Entire Results May Be Viewed.

How can I pause a program so that I may view the entire result?

If a program requires more information than can be displayed at once, users may add a Pause command in the program to pause it until they are ready to continue. This is especially useful when displaying long lists, matrices, etc.

To find Pause locate the pause command:

1) Press Catalog.
2) Press P and select Pause.

If the result of an expression are too large to fit on a single screen, users can use the cursor pad to scroll the display. The program will resume when [ENTER] is pressed.

Users may add an expression after the Pause command to have it display the expression on the Program I/O screen. Expressions can include conversion operations such as >DD and >Rect. Users can also use the  > operator to perform unit and number base conversions.

Please Note: The pause command cannot be used in a user defined-function.

Please see the TI-89 family, TI-92 family and Voyage™ 200 guidebooks for additional information.