Education Technology

Knowledge Base Search

< Previous | 1550 - 1575 of 1765 results |  Next >

Solution 13326: Using the RandSeed Function on the TI-89 Family, TI-92 Family and Voyage™ 200 Graphing Calculators.

...ily, TI-92 family and Voyage 200 graphing calculator? The RandSeed function can be found under the Math menu and under Probability. The proper syntax for using the RandSeed function is listed below: RandSeed number The RandSeed function sets the seed value for the random-number generator function...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/13326

Solution 12651: Clearing the Memory on the TI-81.

...lected, the memory of the graphing calculator is erased and all defaults are set to factory defaults. If the screen goes entirely blank after this procedure, adjust the contrast by pressing and releasing the [2nd] key and then holding down the up arrow until the cursor is again visible. Solution...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/12651

Solution 12648: Calculating Linear Regressions on the TI-81.

... Knowledge Base Search How do I calculate a Linear Regression using the TI-81? The example below will demonstrate how to perform a linear regression using the TI-81: Data for this example:xStat: {1,4,8,10}yStat: {7,9,15,18} Enter the data into the TI-81:1) Enter STAT edi...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/12648

Solution 14240: Converting Between Fractions and Decimals on the TI-73 Explorer™.

... 3) Enter 3 and press [UNIT] [1] [b/c] [A b/cd/e] [ENTER] Example 4: Converting an improper fraction to a decimal. 4) Press [A b/cd/e] [ENTER] More information on converting between decimals and fractions can be found in the TI-73 Explorer guidebook. Solution 14240: Converting Between Fractions...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/14240

Solution 11830: Correcting a Window Variables Domain Error on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.

...domain error on the TI-89 family, TI-92 family, and Voyage 200 graphing calculators? The Window variables domain error occurs when the minimum value for x or y is larger than the maximum value. Edit the window values to resolve this error. Refer to the instructions below. • Press [♦][WINDOW] •...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/11830

Solution 12171: Use of the Angle( Function on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.

...turn p/4.• In Radian mode,angle({0+2i,3+0i,0+4i})[ENTER] will return {p/2 0 -p/2} Please see the TI-89 family, TI-92 family and Voyage 200 guidebooks for additional information. Solution 12171: Use of the Angle( Function on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators. ...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/12171

Solution 16510: How To draw a vertical line on a TI-86.

...a vertical line on a TI-86? To draw a vertical line on the TI-86, there are two options: First on the graph itself: •  Press [MORE]. •  Press [F2] for the Draw function. •  Press [F3] for the Vertical line. •  Use the left and right arrows to move the line to where you want it. •  Press [ENTER...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/16510

Solution 15462: Integrating Lower and Upper Bounds of a Function on the TI-89 Family, TI-92 Family, or Voyage™ 200 Graphing Calculators.

...e^(X^2), X, 0, 1) Press [Enter] to integrate. The answer should be 1.46265174591. Please see the TI-89 family, TI-92 family and Voyage 200 guidebooks for additional information. Solution 15462: Integrating Lower and Upper Bounds of a Function on the TI-89 Family, TI-92 Family, or Voyage™ 200 Gra...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/15462

Solution 11803: Viewing the Top or Bottom of a Large Matrix Result on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.

...rrow so that the visible part of the matrix is highlighted. • Press and hold the shift key (Up Arrow), which is locate to the right of the [2nd] key (For the TI-92 family and Voyage 200, the shift key is located above the ON key). • Then press the up cursor (to scroll up) or the down cursor (to s...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/11803

Solution 12054: Finding the Curl of a Vector Field on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.

...[8] [8] [Y] [=] [2]. 18) Press [2nd] [5] [8] [8] [Z] [=] [1]. 19) Press [ENTER]. Please see the TI-89 family, TI-92 family and Voyage 200 guidebooks for additional information. Solution 12054: Finding the Curl of a Vector Field on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calcula...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/12054

Solution 12097: Graphing Multiple Functions from the Home Screen on the TI-89 Family, TI-92 Family, or Voyage 200™ Graphing Calculators.

...ulator? Multiple functions can be graphed from the home screen on the TI-89 family, TI-92 family, or Voyage 200 using the Store and Graph commands. For example, to graph y=x, y=2x, y=3x from the home screen, Store the functions that will be graphed to a variable {x, 2x, 3x}->glist(x) Use t...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/12097

Solution 11797: Using the Expand() Function on the TI-89 Family, TI-92 Family and Voyage™ 200 Graphing Calculators.

...mily, TI-92 family and Voyage 200 graphing calculators is the exact opposite function of the factor() function. The expansion is polynomial expansion for polynomials and partial fraction expansion for rational expressions. The proper syntax for the expand() function is: expand(expression [,var]...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/11797

Solution 11861: The d() Function Algorithm on the TI-89 Family, TI-92 Family and Voyage™ 200 Graphing Calculators.

...an expression with respect to a variable. The expression can be a list or a matrix. This function uses the chain rule together with the well-known formulas for the derivatives of sums, products, sinusoids, etc. The syntax for this function is: For an Expression: d(expression, var [,order])For...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/11861

Solution 11744: Entering Absolute Values on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.

...Press the [CATALOG] key - [2nd] [CATALOG] on the TI-92 Family and Voyage 2002) Scroll to abs( and press [ENTER]3) Press [(-)] [9] [)]4) Press [ENTER] for the resultPlease see the TI-89 family, TI-92 family and Voyage 200 guidebooks for additional information. Solution 11744: Entering Absolute Va...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/11744

Solution 12125: Converting a Number from Decimal to a Binary Number on the TI-89 Family, TI-92 Family, and Voyage 200™ Graphing Calculators.

...ily, and Voyage 200 graphing calculators? Use the >Bin operator to convert a number to binary. The operator is under the MATH/Base Menu. The syntax for the operator is integer>Bin. Example: Enter 256 >Bin and press [ENTER] to return 0b100000000. Please Note: Binary numbers always have a 0b...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/12125

Solution 11741: Displaying the Correlation Coefficient (R) and Coefficient of Determination (R^2) on the TI-89 Family, TI-92 Family and Voyage™ 200 Graphing Calculators.

... 200 graphing calculators to display the correlation coefficient and coefficient of determination? The correlation coefficient will only be displayed for linear regression calculations (LinReg). The coefficient of determination will be displayed for all polynomial regression calculations (QuadReg...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/11741

Solution 11734: Creating Repetition in a TI Basic Program on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.

...and Voyage 200? There are three structures that allow to program tasks that repeat. The three repetition structures are: • The Loop...EndLoop. • The For ...EndFor. • The While...EndWhile. Each structure is different in its use and provide a unique advantage. Use the Loop..EndLoop when the numb...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/11734

Solution 12120: Clearing All Variables on the TI-89 Family, TI-92 Family, and the Voyage™ 200 Graphing Calculator.

...e Search How do I reset all the variables back to zero on my TI-89 family, TI-92 family, or Voyage 200 graphing calculator? The instructions for clearing all variables and resetting them back to the default value on the TI-89 family, TI-92 family, or Voyage 200 graphing calculator have b...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/12120

Solution 10422: Creating Box Plots Using the TI-86.

...wledge Base Search How do I create a box plot on the TI-86? The example below will demonstrate how to create a box plot on the TI-86. Data for this example: xStat: {3,5,8,10} fStat: {7,8,14,18} To enter the data into the TI-86: • Enter STAT mode by pressing [2nd] [STAT]. • Press [F2]...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/10422

Solution 11727: Computing the Dot Product on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.

...Both vectors must have equal dimension, and the dimension must be either 2 or 3. Please see the TI-89 family, TI-92 family, and Voyage 200 guidebooks for additional information. Solution 11727: Computing the Dot Product on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators. ...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/11727

Solution 11725: Computing the Cross Product on the TI-89 Family and Voyage™ 200 Graphing Calculators.

...ly and Voyage 200 calculators? The following instructions demonstrate how to compute the cross product using a TI-89 Family or Voyage 200 calculator: For Example: Find the cross product of vectors and 1) Turn the calculator ON and on the TI-89 Family press [HOME] and on the Voyage 200 press [Gr...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/11725

Solution 11714: Calculating the Eigenvalue and Eigenvector of a Matrix on the TI-89 Family, and Voyage™ 200 Graphing Calculators.

...phing calculators? To calculate the eigenvalue and eigenvector of a matrix on the TI-89 family, and Voyage 200 refer to the instructions below:Matrix for this example is: [  5  3  12] [  6  1  5  ][  0  6  -2 ]To create the matrix, press [HOME] to return to the main screen of the calculator and f...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/11714

Solution 12114: Calculating Integrals on the TI-89 Titanium and Voyage™ 200 Graphing Calculators.

... Search How do I calculate integrals on the TI-89 Titanium and Voyage 200 graphing calculators? The following examples demonstrate how to perform indefinite and definite integrals on the TI-89 Titanium and Voyage 200 graphing calculators: Indefinite integrals: Please Note: The ∫ symbol...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/12114

Solution 10579: Entering Absolute Values using the TI-85 and TI-86 Graphing Calculators.

...the abs function to obtain the absolute value using the TI-85 and TI-86. Example: Find |-6| • Press [2nd][MATH][F1][F5] • Input -6 • Press [ENTER] for the result For further information, please refer to the TI-85 or TI-86 Guidebooks. Solution 10579: Entering Absolute Values using the TI-85 a...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/10579

Solution 10404: Table Feature on the TI-85.

...ed program. Texas Instruments does not directly provide programs, although you may be able to locate a third-party program by conducting a web search.For instructions on using each specific program, refer to the documentation that is located with the program file. This documentation will have d...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/10404