Knowledge Base Search
Solution 10417: Calculating Two-Variable Statistics on the TI-86
...e it blank.) 4) Press [2nd] [QUIT] to leave the editor.Calculate the statistical variables:1) Press [2nd] [STAT] [F1] [F2]; the function TwoVar will appear on the screen. 2) Press [2nd] [LIST] [F3] to see the list names in the menu. 3) Select xStat [,] yStat [ENTER] the screen will now show the ...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/10417
Solution 10424: Degree, Minutes, Seconds (DMS) Conversions with the TI-85 or TI-86.
...ed using a single quote after each value. For example, 15'12'8' would be interpreted as 15 degrees, 12 minutes and 8 seconds. The ' symbol can be accessed by pressing [2nd] [MATH] [F3:ANGLE] [F3:']. To convert a number that is written in decimal degrees to DMS, use the [>DMS] function, found...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/10424
Solution 11831: Correcting an Address Error on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.
...ons below will detail how to correct the Address Error on the TI-89 family, TI-92 family, and Voyage 200 calculators. Please Note: The following procedures will completely reset the calculator. Please, bear in mind that this will erase the memory of the calculator and restore all manufacturer's...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/11831
Solution 11827: Calculating the Determinant of a Matrix Using the TI-89 Family, TI-92 Family and Voyage™ 200 Graphing Calculators.
... select Data/Matrix Editor, and press [3]). 2) The Type: will be Matrix, input b for the Variable: and the dimensions are both 3. 3) Press [ENTER] twice. 4) Input the values that are above in the data matrix editor. Go to the home screen and input det(b). Press [ENTER] for the solution. Please...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/11827
Solution 11826: Calculating nth Power and Roots Using the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.
...( function will populate in the entry line. 2) Input 27, press [,] and enter 3. 3) Press [)] [ENTER]. The screen will display 3. Please Note: It is necessary to put parentheses around the negative number because these calculators evaluate negation with the same priority as multiplying by a negati...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/11826
Solution 12170: Using the "and" Operator on TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.
...I-89 family, TI-92 family, and Voyage 200 graphing calculators? The and operator is primarily used to compare two Boolean expressions, lists, or matrices and returns true, false, or a simplified form of the original entry. When used with integers, the and operator compares them bit-by-bit using a...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/12170
Solution 11822: Algorithm Used for the propFrac() Function on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.
Solution 11822: Algorithm Used for the propFrac() Function on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators. Solution 11822: Algorithm Used for the propFrac() Function on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators. global Solution 11822: Al...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/11822
Solution 11820: Algorithm Used for the cZeros() (Complex Zeros) Function on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.
Solution 11820: Algorithm Used for the cZeros() (Complex Zeros) Function on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators. Solution 11820: Algorithm Used for the cZeros() (Complex Zeros) Function on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators. ...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/11820
Solution 12663: Entering Numbers in Scientific Notation on a TI-89 Family, TI-92 Family and Voyage™ 200 Graphing Calculator.
...amily, TI-92 family or Voyage 200 graphing calculator? A number can be entered using scientific notation with the use of the EE function, which is accessed by pressing [EE] which is used to represent x10. Example: Input 2.5 x 105 and display the results in standard form Solution: • Input 2.5 • ...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/12663
Solution 12138: Font and Size of Characters Used on the TI-89 Family, TI-92 Family and Voyage™ 200 Graphing Calculators.
...a custom set that gets installed on the PC along with most of Texas Instruments' Windows® applications (such as NoteFolio Creator™). It is called Ti92Pluspc on the computer. On the calculator, most of the characters are 5 pixels wide by 7 pixels high in the body of the display screen. The small f...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/12138
Solution 12134: Using Strings on the TI-89 Family, TI-92 Family, and Voyage™ 200.
...edge Base Knowledge Base Search How are strings used on the TI-89 Family, TI-92 Family, and Voyage 200? Strings are a sequence of characters enclosed in "quotes". Strings are used to enter and display text characters. Strings can be entered directly or stored to a string...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/12134
Solution 11815: Finding a Maximum or Minimum of a Function on a TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculator.
...ind the maximum or minimum value of a function using a TI-89 family, TI-92 family, or Voyage 200? To calculate a maximum or minimum of a function, access the Math menu after graphing a function. Then, from the menu that appears, select the calculation to be performed. The example below will demo...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/11815
Solution 12096: Graphing a Step Function on the TI-89 Family, TI-92 Family, or Voyage™ 200 Graphing Calculators.
...h the greatest integer of Y=X 1) Go to the Y= editor screen by pressing the [GREEN DIAMOND][W]. (Use [GREEN DIAMOND] [F1] on the TI-89 Family). 2) Access the catalog by pressing [2nd] [2] (on the TI-89 press [CATALOG]). 3) Press the [I] key to go to the "I" commands. 4) Scroll to the int( comman...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/12096
Solution 12092: Creating a Scatter Plot Using the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.
...lators? The following example will demonstrate how to create a scatter plot using the TI-89, TI-92 Family, and Voyage 200. Data for example: Access the data matrix editor: 1) Press [APPS] [6] [3] (If the Apps Desktop is on, press [APPS], select Data/Matrix Editor, and choose [3].) 2) Scr...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/12092
Solution 12091: Creating a Histogram Using the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.
...Input the data • Press [APPS] [6] [3]. (If the Apps Desktop is on, press [APPS], select Data/Matrix Editor, and choose [3].)• Press the down arrow twice. • In the box beside variable type a variable name. (e.g. TEST) • Press [ENTER] [ENTER].• Enter the numbers for the x values under c1. Press [5]...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/12091
Solution 11852: Algorithm for tCollect() Function on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.
Solution 11852: Algorithm for tCollect() Function on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators. Solution 11852: Algorithm for tCollect() Function on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators. global Solution 11852: Algorithm for tColle...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/11852
Solution 12058: Fractions with the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.
... returns fractional results in the form of an improper fraction. Use propFrac() function to return an improper fraction as a mixed number, which is accessed by pressing [2nd][MATH][9][7]. Please Note: Before trying the examples below, enter the [MODE] menu and change the Exact/Approximate settin...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/12058
Solution 14289: Backing Up the Memory of a TI-73 Family Calculator by Saving to Another TI-73 Family Model.
... How do I back up the memory from one TI-73 or TI-73 Explorer to another? The TI-73 family calculator includes two types of memory: RAM (Random Access Memory) and F-ROM (Flash Read Only Memory). RAM includes all lists, programs, variables and equations. F-ROM includes software applications (A...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/14289
Solution 35134: Calculating Present Value (PV) on the TI-89 Family, TI-92 Family, and Voyage™ 200.
...o I calculate present value (PV) on the TI-89 Family, TI-92 Family, and Voyage 200? Press the [APPS] button on the handheld and then select the [Finance] Application Example: • Input the number of payments (10) on N= 10.00 and press [ENTER] • Input interest rate per payment period (10) on I/Y...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/35134
Solution 12057: Fraction to Decimal Conversions on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.
...n to a decimal: 1) Press [MODE]. 2) Scroll to Exact/Approx. 3) Choose Approximate. 4) Input a fraction and press [ENTER]. For mixed numbers, the procedure is the same as for fractions. However, the mixed number has to be entered as a sum. For example, for two and three fourths, enter (2+3/4). ...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/12057
Solution 12079: Creating Truth Tables Using the TI-89 Family, TI-92 Family, and Voyage™ 200.
... For an example truth table, follow the steps below: 1) Create a list called A with the numbers 0, 1, 0 and 1. To do this, press [HOME] (on the TI-92 Plus and Voyage 200, press [♦] [Q]), input {0,1,0,1}, then press [STO->] [ALPHA] [A] [ENTER]. 2) Create a list called B with the numbers 0, 0, 1 an...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/12079
Solution 12059: Implicit Partial Differentiation on the TI-89 Family, TI-92 Family, or Voyage™ 200 Graphing Calculators.
...nd TI-89 Titanium operating system contain a impdif ( command. This command should be used when computing a implicit partial differentiation. To access the command, press [F3] [Up Arrow] [Enter] on the homescreen. For example, to solve the equation x^2+y^2=0, enter impdif(x^2+y^2=0, x, y) and...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/12059
Solution 12069: Storing a Value to a Matrix Element on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.
...3) To create the matrix above, the Type: will be Matrix, the Variable: name is A, and the row and column dimensions are both 2. 4)Press [ENTER] twice. 5) Input the values that are above in the Data/Matrix Editor in sequence from left to right. If "A" is a 2x2 matrix, then to store the value o...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/12069
Solution 12046: Calculating Two-Variable Statistics on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.
...PPS] use the arrows to select [Data/Matrix Editor] and press [ENTER]. 2) Choose [3: New] then press [Enter]. 3) Press [Down Arrow] [Down Arrow] to place the cursor in the variable box then enter a variable name for example: datab. 4) Press [ENTER] [ENTER] to open the editor. 5) Enter the x value...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/12046
Solution 11806: Creating and Evaluating User-Defined Functions on the TI-89 Family, TI-92 Family and Voyage™ 200.
...ents for subsequent functions or programs. In the argument list, be sure to use the same arguments that are used in the definition. Arguments are placeholders that represent whatever values passed to the function. Functions can be created using one of the following methods: 1. Using the [STO->...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/11806