Education Technology

Knowledge Base Search

< Previous | 1000 - 1025 of 1414 results |  Next >

Solution 12170: Using the "and" Operator on TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.

...I-89 family, TI-92 family, and Voyage 200 graphing calculators? The and operator is primarily used to compare two Boolean expressions, lists, or matrices and returns true, false, or a simplified form of the original entry. When used with integers, the and operator compares them bit-by-bit using a...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/12170

Solution 15689: Entering Numbers Using Scientific Notation on a TI-85 and TI-86 Graphing Calculator.

...in scientific notation on a TI-85 or TI-86 calculator? A number can be entered using scientific notation with the use of the EE function, which is accessed by pressing [EE]. This key represents x10. Example: Input 1.5 x 108 and display the results in standard form. Solution:• Input 1.5.• Press [...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/15689

Solution 12663: Entering Numbers in Scientific Notation on a TI-89 Family, TI-92 Family and Voyage™ 200 Graphing Calculator.

...amily, TI-92 family or Voyage 200 graphing calculator? A number can be entered using scientific notation with the use of the EE function, which is accessed by pressing [EE] which is used to represent x10. Example: Input 2.5 x 105 and display the results in standard form Solution: • Input 2.5 • ...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/12663

Solution 11819: Algorithm for Solving Systems of Equations on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.

.... For linear or polynomial systems, the Gaussian or Groebner elimination method is used to seek all solutions. Otherwise, a damped-Newton/steepest-descent method is used to seek an approximate solution close to the entered guess, which defaults to 0.0 for each component. Solution 11819: Algorith...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/11819

Solution 12138: Font and Size of Characters Used on the TI-89 Family, TI-92 Family and Voyage™ 200 Graphing Calculators.

...a custom set that gets installed on the PC along with most of Texas Instruments' Windows® applications (such as NoteFolio Creator™). It is called Ti92Pluspc on the computer. On the calculator, most of the characters are 5 pixels wide by 7 pixels high in the body of the display screen. The small f...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/12138

Solution 15468: Unlocking a Program on the TI-89 Family, TI-92 Family and Voyage™ 200 Graphing Calculators.

...Base Search How can I unlock a program on the TI-89 Family, TI-92 Family, and Voyage 200? Program authors usually lock programs to prevent access or modification to the existing programming code. However, a program can be unlocked on the TI-89 Family, TI-92 Family and Voyage 200 calculat...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/15468

Solution 11818: Algebra Problem Identities for 00 using the TI-89 Family, TI-92 Family, or Voyage™ 200 Graphing Calculators.

...ion of ones, or an empty collection of twos, etc. Therefore, 00 = 10 = 20 = x0 = 1. Finally, note that limits are not relevant to the discussion. Since the function f(x,y) = xy has an essential discontinuity at (0,0), no choice of f(0,0) will make the function continuous there. That does not, ho...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/11818

Solution 12134: Using Strings on the TI-89 Family, TI-92 Family, and Voyage™ 200.

...edge Base Knowledge Base Search How are strings used on the TI-89 Family, TI-92 Family, and Voyage 200? Strings are a sequence of characters enclosed in "quotes". Strings are used to enter and display text characters. Strings can be entered directly or stored to a string...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/12134

Solution 11815: Finding a Maximum or Minimum of a Function on a TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculator.

...ind the maximum or minimum value of a function using a TI-89 family, TI-92 family, or Voyage 200? To calculate a maximum or minimum of a function, access the Math menu after graphing a function. Then, from the menu that appears, select the calculation to be performed. The example below will demo...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/11815

Solution 12096: Graphing a Step Function on the TI-89 Family, TI-92 Family, or Voyage™ 200 Graphing Calculators.

...h the greatest integer of Y=X 1) Go to the Y= editor screen by pressing the [GREEN DIAMOND][W]. (Use [GREEN DIAMOND] [F1] on the TI-89 Family). 2) Access the catalog by pressing [2nd] [2] (on the TI-89 press [CATALOG]). 3) Press the [I] key to go to the "I" commands. 4) Scroll to the int( comman...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/12096

Solution 15463: Finding the Amplitude of Periodic Function on the TI-89 Titanium and Voyage™ 200 Graphing Calculators.

... Knowledge Base Search How do I find the amplitude of a periodic function? The amplitude of a periodic function is one-half the difference between the largest possible value of the function and the smallest possible value. For example, for y= sin(x), the largest possible value of y ...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/15463

Solution 11805: Negative Exponents of Zero Return Inconsistent Answers on the TI-89 Family, TI-92 Family and Voyage™ 200.

...exponent: 0^-1 solution "undef" 0^-2 solution infinity 0^-3 solution "undef" 0^-4 solution infinity etc... The answer should always be undefined since (0/1)^-n is (1/0)^n. Solution 11805: Negative Exponents of Zero Return Inconsistent Answers on the TI-89 Family, TI-92 Family and Voyage™ 200...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/11805

Solution 12092: Creating a Scatter Plot Using the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.

...lators? The following example will demonstrate how to create a scatter plot using the TI-89, TI-92 Family, and Voyage 200. Data for example:   Access the data matrix editor:  1) Press [APPS] [6] [3] (If the Apps Desktop is on, press [APPS], select Data/Matrix Editor, and choose [3].) 2) Scr...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/12092

Solution 15320: Performing Order of Magnitude on the TI-86 Graphing Calculator.

...the value and press [ENTER]The antilog of the log is 10 raised to the power of that number. For example, the antilog of 2 is 10^2. This function is accessed by pressing [2nd] [LOG].Please see the TI-86 guidebook for additional information. Solution 15320: Performing Order of Magnitude on the TI-...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/15320

Solution 12091: Creating a Histogram Using the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.

...Input the data • Press [APPS] [6] [3]. (If the Apps Desktop is on, press [APPS], select Data/Matrix Editor, and choose [3].)• Press the down arrow twice. • In the box beside variable type a variable name. (e.g. TEST) • Press [ENTER] [ENTER].• Enter the numbers for the x values under c1. Press [5]...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/12091

Solution 15300: Calculating Factorials on the TI-85 and TI-86 Graphing Calculators.

... Knowledge Base Knowledge Base Search How do I calculate factorials on a TI-85 or TI-86 graphing calculator? The procedure below will demonstrate how to calculate factorials on a TI-85 or TI-86 graphing calculator. Example: Compute 5! • Enter 5 and press [2nd] [F...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/15300

Solution 11795: Using the deSolve() Function on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.

...ily and [♦] [Q] on the TI-92 family and Voyage 200. 2) Press [F3] and select C:deSolve( 3) Input the expression y'=10y*(y-25) Please Note: The ' is accessed by pressing [2nd][=] on the TI-89 family and [2nd][B] on the TI-92 family and Voyage 200. Enter the multiplication symbol as denoted by the ...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/11795

Solution 14488: Rules for Variable Names on the TI-89 Titanium and Voyage™ 200.

...-89 Titanium or Voyage 200: • A variable name can use 1 to 8 characters consisting of letters and digits. This includes Greek letters (but not p), accented letters, and international letters. Do not include spaces. The first character cannot be a digit. • Variable names can use uppercase and low...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/14488

Solution 11842: Algorithm Used for Symbolic Integration Function on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.

...pe algorithms. Definite integrals are determined by subdividing the interval at detected singularities, then for each interval, computing the difference of the limit of an antiderivative at the upper and lower integration limits. Except in exact mode, nInt() is used were applicable when symbolic ...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/11842

Solution 14485: Modifying the History Area on the TI-89 Titanium and Voyage™ 200 Graphing Calculators.

...lowed by the [|] key. 2) Press the right arrow key. 3) Use the up or down arrow keys to highlight the new number of pairs desired. • Press [ENTER] twice. 2. Clearing the history area and deleting all saved pairs: 1) From the Calc Home screen, press [F1]. 2) Select 8:Clear Home or enter ClrHome ...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/14485

Solution 12058: Fractions with the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.

... returns fractional results in the form of an improper fraction. Use propFrac() function to return an improper fraction as a mixed number, which is accessed by pressing [2nd][MATH][9][7]. Please Note: Before trying the examples below, enter the [MODE] menu and change the Exact/Approximate settin...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/12058

Solution 14289: Backing Up the Memory of a TI-73 Family Calculator by Saving to Another TI-73 Family Model.

... How do I back up the memory from one TI-73 or TI-73 Explorer to another? The TI-73 family calculator includes two types of memory: RAM (Random Access Memory) and F-ROM (Flash Read Only Memory). RAM includes all lists, programs, variables and equations. F-ROM includes software applications (A...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/14289

Solution 12081: Graphing Inequalities on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.

...: Graph y<=3x+2 On the graphing calculator:  1) Press [Diamond Key] [Y=], and next to y1=, input 3x+2 then press [ENTER].  2) Press the [Up Arrow] once to highlight the "3x+2". 3) Press [2nd] [F1] to open the "Style" menu and press [8] to select 8:Below. 4) Press [Diamond Key] [F3] to view the s...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/12081

Solution 35134: Calculating Present Value (PV) on the TI-89 Family, TI-92 Family, and Voyage™ 200.

...o I calculate present value (PV) on the TI-89 Family, TI-92 Family, and Voyage 200? Press the [APPS] button on the handheld and then select the [Finance] Application Example: • Input the number of payments (10) on N= 10.00 and press [ENTER] • Input interest rate per payment period (10) on I/Y...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/35134

Solution 12057: Fraction to Decimal Conversions on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.

...n to a decimal: 1) Press [MODE]. 2) Scroll to Exact/Approx. 3) Choose Approximate. 4) Input a fraction and press [ENTER]. For mixed numbers, the procedure is the same as for fractions. However, the mixed number has to be entered as a sum. For example, for two and three fourths, enter (2+3/4). ...
https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/12057