Knowledge Base Search
Solution 10449: Using the Interpolate Editor on the TI-85 and TI-86.
...NTER]. • At x2=, input -1 and press [ENTER]. • At y2=, input -2 and press [ENTER]. • At x=, input 7 and press [ENTER]. • At y=, press [F5] to solve for the y value. The calculator should display 14 as the solution. Please see the TI-85 and TI-86 guidebooks for additional information. Solution...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/10449
Solution 10401: Plotting Points using the TI-85.
...earch How do I plot a set of points using the TI-85? The following example will demonstrate how to plot a set of points using the TI-85:Data for this example: xStat: {3,5,8,10}yStat: {7,8,14,18}1) Clear the screen then press [STAT] [F2] [F1] [ENTER] [ENTER].2) The cursor will display aft...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/10401
Solution 10439: Plotting Points Using the TI-86.
...arch How do I plot a set of points using the TI-86? The following example will demonstrate how to plot a set of points using the TI-86:Data for this example:xStat: {3,5,8,10}yStat: {7,8,14,18}Enter the data into the TI-86:• Enter STAT mode by pressing [2nd][STAT].• Press [F2] to select ...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/10439
Solution 10426: Finding the Intersection of Functions on the TI-85 or TI-86.
Solution 10426: Finding the Intersection of Functions on the TI-85 or TI-86. Solution 10426: Finding the Intersection of Functions on the TI-85 or TI-86. global Solution 10426: Finding the Intersection of Functions on the TI-85 or TI-86. website ...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/10426
Solution 10372: Calculating Numeric Derivatives on the TI-82.
Solution 10372: Calculating Numeric Derivatives on the TI-82. Solution 10372: Calculating Numeric Derivatives on the TI-82. global Solution 10372: Calculating Numeric Derivatives on the TI-82. website Ho...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/10372
Solution 10356: Solving Simultaneous Equations on the TI-85 or TI-86.
... The example below will demonstrate how to use the SIMULT function to solve simultaneous equations on the TI-85 or TI-86.Example: Solve the following for x, y and z.3x + 3y - 4z = -3-x + 2y + 5z = 188x + 4y - 7z = -5Solution:1) Press [2nd] [SIMULT]2) Input 3 (This indicates that there are three e...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/10356
Solution 10351: Finding the Inverse of a Matrix on the TI-85 or TI-86 Graphing Calculator.
...7](MATRX) [F2] to enter the matrix editor. 2) Input [A] press [ENTER] 3) Input the dimensions of the matrix (2 [ENTER] 2 [ENTER]) 4) Input the values for the elements of the matrix pressing [ENTER] after each entry 5) Press [Exit] to return to the home screen To find the inverse of matrix A: 1) ...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/10351
Solution 18709: Calculating the gcd() (Greatest Common Divisor) on the TI-85 and TI-86 Graphing Calculators.
... the list, and a list is returned. The syntax is as follows: gcd(valueA,valueB) gcd(listA,listB) Examples: • Find the greatest common divisor for lists A and B: {12,14,16}, {9,7,5} • Find the greatest common divisor for 36 and 280. The gcd() function can be located by following the keys...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/18709
Solution 11754: Finding the Complex Conjugate of an Imaginary Number on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.
... {2-3i, i, 1+i}• conj([9, 2-i; 1-i, -i] will return the matrix [9, 2+i; 1+i, i]. The matrix will be in pretty print if Pretty Print mode is turned ON.For additional instructions, refer to the online guidebook for your calculator. Solution 11754: Finding the Complex Conjugate of an Imaginary Numb...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/11754
Solution 10379: Finding the Zero of a Function using the TI-82.
Solution 10379: Finding the Zero of a Function using the TI-82. Solution 10379: Finding the Zero of a Function using the TI-82. global Solution 10379: Finding the Zero of a Function using the TI-82. website ...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/10379
Solution 11750: Finding an Intersection of Functions on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.
... key, [F1]. 2) Input the equations. 3) Press the diamond key, [F3]. The graphs are now displayed on the screen. Find the intersection: 1) Press [F5] for the Math menu and select 5:Intersection 2) Select the first function using the up or down cursor and press [ENTER] 3) Set the second function ...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/11750
Solution 17169: Calculating the Second Derivative and Antiderivative Using a TI-89 Family, TI-92 Family and Voyage™ 200 Graphing Calculator.
...-89 family, TI-92 family or Voyage 200 calculator? The differentiate command, d (differentiate), computes derivatives. Please see the below example for computing the second derivative: Example: What is the second derivative of 3x5? 1) Press [F3][1] to select 1:d( differentiate. 2) Enter 3x^5) a...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/17169
Solution 11715: Calculating the Inverse Natural Log on the TI-89 Family, TI-92 Family or Voyage™ 200 Graphing Calculators.
...iamond] [ex][1] [)] [Green Diamond][ENTER]. The answer 2.71828 will be displayed. Please see the TI-89 family, TI-92 family and Voyage 200 guidebooks for additional information. Solution 11715: Calculating the Inverse Natural Log on the TI-89 Family, TI-92 Family or Voyage™ 200 Graphing Calculato...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/11715
Solution 10348: Calculating Inverse Trigonometric Functions on the TI-85 or TI-86 Graphing Calculators.
...nctions are calculated in angle measurements of degrees. The steps outlined below will change the mode from the default setting of radians to degrees for the measurement of angles. However, if this step is omitted the measure of the angle may be in radians and not degrees. • Press [2nd] [MODE] ...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/10348
Solution 11593: Defining a Function from a Program Prompt on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.
...ymbol, press the [STO>] key. To input the "&" symbol, press [2nd] [CHAR] [3] [6]. Please see the TI-89 family, TI-92 family and Voyage 200 guidebooks for additional information. Solution 11593: Defining a Function from a Program Prompt on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/11593
Solution 11701: Calculating Combinations and Permutations on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing Calculators.
... 2) Press [2nd][MATH][7][2] 3) Press [5][,][2][ENTER] The screen will show 20. Please see the TI-89 family, TI-92 family and Voyage 200 guidebooks for additional information. Solution 11701: Calculating Combinations and Permutations on the TI-89 Family, TI-92 Family, and Voyage™ 200 Graphing...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/11701
Solution 10418: Converting Mixed Numbers into Improper Fractions on a TI-85 or TI-86 Graphing Calculator.
...calculator. Example: Convert 1 3/5 into an improper fraction: 1) Press [1] [+] [3] [¸] [5] on the HOME screen. 2) Press [2nd][MATH]. 3) Press [F5] for MISC and [MORE]. 4) Now, press [F1] to select >FRAC. 5) Press [ENTER]. The screen will display 8/5. Please see the TI-85 and TI-86 guidebooks...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/product-usage/10418
Solution 12308: Converting Fractions to Decimals on the TI-36X Solar.
Solution 12308: Converting Fractions to Decimals on the TI-36X Solar. Solution 12308: Converting Fractions to Decimals on the TI-36X Solar. global Solution 12308: Converting Fractions to Decimals on the TI-36X Solar. website ...https://education.ti.com/en/customer-support/knowledge-base/scientific-elem-calculators/product-usage/12308
Solution 12316: Utilizing Memory Functions on the TI-36X Solar.
...entary & basic calculators Knowledge Base Knowledge Base Search How do I use memory functions on the TI-36X Solar? The procedures below describe how to use the memory functions on the TI-36X Solar.Store Key Sequence:With the number to be stored in the display of the ca...https://education.ti.com/en/customer-support/knowledge-base/scientific-elem-calculators/product-usage/12316
Solution 33451: Calculating Combinations and Permutations on the TI-36X Pro.
Solution 33451: Calculating Combinations and Permutations on the TI-36X Pro. Solution 33451: Calculating Combinations and Permutations on the TI-36X Pro. global Solution 33451: Calculating Combinations and Permutations on the TI-36X Pro. website ...https://education.ti.com/en/customer-support/knowledge-base/scientific-elem-calculators/product-usage/33451
Solution 33652: Creating a Matrix on the TI-36X Pro Scientific Calculator.
Solution 33652: Creating a Matrix on the TI-36X Pro Scientific Calculator. Solution 33652: Creating a Matrix on the TI-36X Pro Scientific Calculator. global Solution 33652: Creating a Matrix on the TI-36X Pro Scientific Calculator. website ...https://education.ti.com/en/customer-support/knowledge-base/scientific-elem-calculators/product-usage/33652
Solution 12327: Calculating Inverse Logarithms on the TI-30Xa Family and TI-36X Solar Scientific Calculators.
...5. 1) Enter .5 and press [2nd] [LOG] (10x is labeled above it). The answer is 3.16227766. Please see the TI-30Xa family and TI-36X Solar guidebooks for additional information. Solution 12327: Calculating Inverse Logarithms on the TI-30Xa Family and TI-36X Solar Scientific Calculators. ...https://education.ti.com/en/customer-support/knowledge-base/scientific-elem-calculators/product-usage/12327
Solution 12328: Calculating Logarithms Using the TI-30Xa Family or TI-34.
...ess [7] [3] [LOG].The calculator will display 1.86332286.To calculate logarithms with a base different than 10, you may use the following workaround: For example, to calculate the log base 4 of 1601) Input [160] Press [LOG].2) Press [÷].3) Input [4] Press [LOG].4) Press [=] to complete the calcul...https://education.ti.com/en/customer-support/knowledge-base/scientific-elem-calculators/product-usage/12328
Solution 15301: Resetting the TI-30X IIS/B.
Solution 15301: Resetting the TI-30X IIS/B. Solution 15301: Resetting the TI-30X IIS/B. global Solution 15301: Resetting the TI-30X IIS/B. website Home | Scientific, elementary & basic calculators Knowl...https://education.ti.com/en/customer-support/knowledge-base/scientific-elem-calculators/product-usage/15301
Solution 12112: Battery Life of Voyage™ 200 Graphing Calculator.
...e Base Search How long do the AAA batteries last in the Voyage 200? Voyage 200 battery life will vary based on the types of computations performed and programs that are being used. Typically the battery life will last well beyond a school year. The Voyage 200 uses four AAA batteries for...https://education.ti.com/en/customer-support/knowledge-base/other-graphing/general-information/12112