Education Technology

Battery Regulatory

Regulatory Battery Caution:

  • Do not ingest battery, Chemical Burn Hazard.
  • Keep new and used batteries away from children.
  • Always completely secure the battery compartment. If the battery compartment does not close securely, stop using the product, remove the batteries, and keep them away from children.
  • If you think batteries might have been swallowed or placed inside any part of the body, seek immediate medical attention.
  • Call a local poison control center for treatment information.
  • Even used batteries may cause severe injury or death.
  • Non-rechargeable batteries are not to be recharged.
  • Do not force discharge, recharge, disassemble, heat above 140F (60C) or incinerate. Doing so may result in injury due to venting, leakage or explosion resulting in chemical burns.
  • Ensure the batteries are installed correctly according to polarity (+ and -).
  • Do not mix old and new batteries, different brands or types of batteries, such as alkaline, carbon-zinc or rechargeable batteries.
  • Risk of fire or explosion if battery is replaced by an incorrect type.
  • Remove and immediately recycle or dispose of batteries from equipment not used for an extended period of time according to local regulations. Do NOT dispose of batteries in household trash or incinerate.