Available for purchase at these instructional product dealers.
TI-Innovator™ Hub
The coding platform that students program with TI graphing calculators to explore math, science and STEM principles.
The coding platform that students program with TI graphing calculators to explore math, science and STEM principles.
Available for purchase at these instructional product dealers.
Available for purchase at these retailers.
Plug-and-play and ready-to-use with TI graphing calculators, the
TI-Innovator™ Hub enables students to learn basic coding and design, use those skills to program and build working solutions, and connect STEM concepts.
The TI-Innovator™ Hub supports the TI-84 Plus CE and the
TI-Nspire™ CX families of graphing calculators and software.
Now available on TI-Nspire™ CX II family graphing calculators, enhance physical computing by using Python programming on your handheld to control the
TI-Innovator™ Hub and Rover.
Embed coding and engineering design into engaging math and science lessons with the TI-Innovator™ Hub and TI graphing technology.
TI LaunchPad™ Technology — used by engineers in the field — is built in, giving students early exposure to professional applications.
The TI-Innovator™ Hub is ready out of the box to connect with TI-84 Plus CE and
TI-Nspire™ CX family graphing technology.
Challenge students to solve open-ended problems by building projects with the
Multiple input and output ports expand the TI-Innovator™ Hub capability to motivate students to imagine, design, build and test creative solutions.
Students can write code to program working solutions that actuate a red-green-blue LED, single red LED, light brightness sensor and speaker built into the TI-Innovator™ Hub.
The TI-Innovator™ Hub is enclosed in a durable case that is ready for your classroom.
Required for the Path to STEM Projects activities, this pack contains resistors, capacitors, LEDs and other components for exploring electronics principles.
From motors to sensors, the I/O Modules plug into the input or output ports of the
This adapter allows for connection to four popular Vernier sensors to the TI-Innovator™ Hub. Use the pH, Temperature, Force, or Pressure sensors from Vernier in your TI-Innovator™ activities.
Stay up to date on product updates, activities and more.
Computer OS
Computer hardware
Chrome OS™ is a trademark of Google LLC. Firefox is a trademark of the Mozilla Foundation in the U.S. and other countries. Mac and Safari are trademarks of Apple Inc., registered in the U.S. and other countries. Chrome OS™ is a trademark of Google LLC. Intel and Windows are registered trademarks of their respective owners.
TI-Innovator™ Packs and modules provide the components to extend the capabilities of the TI-Innovator™ Hub with TI LaunchPad™ Board.
Rover is a two-wheeled programmable robotic vehicle that works with the TI-Innovator™ Hub.
Learn moreFrom motors to environmental sensors to LED displays, these modules plug into the input or output ports of the TI-Innovator™ Hub to quickly and easily expand the capabilities of the TI-Innovator™ Hub.
LED and displays
TI-RGB ArrayThe TI-RGB Array contains 16 individually programmable RGB LEDs. Package includes one TI-RGB Array and cable.
White LED five packLight-emitting diode that emits white light. Pack includes five white LED modules and cables. |
Motion sensors
Ultrasonic Ranger ModuleMeasures distance from the module in centimeters. Package includes one Ultrasonic Ranger Module and cable. |
Environmental sensors
Light sensor five packThis sensor detects the light intensity of the environment. Pack includes five light sensors and cables.
Moisture module five packDetects the moisture of soil, to judge if there is dampness around the sensor. Pack includes five moisture sensors and cables.
Temperature five packMeasures ambient temperature. Pack includes five temperature sensors and cables.
Temperature and humidity (DHT) sensor five packSensor that measures relative humidity and the temperature. Pack includes five temperature and humidity (DHT) sensors and cables. |
Actuators and motors
Servo motor five pack360-degree, continuous-rotation servo motor. Pack includes five servo motors.
Vibration motor five packCoin-type motor that vibrates. Pack includes five vibration motors and cables.
Water pump five packSubmergible water pump. Pack includes five water pumps and five sets of tubing. |
Power and signal control
MOSFET module five packPower control components. Pack includes five MOSFET modules and five AA battery holders. |
Other
Hall sensor five packSensor that measures the Hall Effect. Pack includes five hall sensors and cables. |
This convenient collection of LEDs and cables allow exploration of LED-based activities using the breadboard connector of the TI-Innovator™ Hub.
Pack contents:
The TI-Innovator™ Breadboard Pack is ideal for use in exploring electronics principles.

TI-Innovator™ Breadboard Pack contents:
This adapter allows for connection from several popular Vernier sensors to the TI-Innovator™ Hub. Use the pH, Temperature, Force, Pressure, Low-g accelerometer, Light and Energy sensors from Vernier in your TI-Innovator™ activities.* If interested in using other Vernier sensors with the TI-SensorLink Adapter, please contact the TI STEM team at stem-team@ti.com for assistance.
Optional source of power when using components that require extra power.
*The Vernier Energy Sensor requires two TI-SensorLink Adapters connected to the TI-Innovator™ Hub to measure energy (both voltage and current).
Find helpful links to keep your TI-Innovator™ system up to date, online learning opportunities, and project-based learning activities that help students explore, understand and connect the principles of science, math, coding, engineering design and electronics.
Keep your TI-84 Plus CE graphing calculator, TI-Nspire™ CX technology and TI-Innovator™ Hub up to date.
Download the latest product manuals and Getting Started guides to get the most from your TI-Innovator™ Hub.
Open new channels for inquiry, exploration and collaboration with free activities for TI-Innovator™ Technology.
Learn how to effectively use the TI-Innovator™ system and content to engage students in the STEM classroom with these free online webinars.
This searchable TI-Cares™ Knowledge Base provides answers to most questions for the TI-Innovator™ system.
Troubleshoot problems with your TI-Innovator™ Hub, Rover, or I/O Modules with these test programs.
On-board components for:
TI-84 Plus CE graphing calculator
I/O Modules for:
TI-84 Plus CE graphing calculator
Rover for: