Education Technology
play

Defining and entering functions

1.    From the Home Screen select the Function Editor icon or press c to display the Y= editor.

2.    Press the down arrow to move the cursor to the function you want to define or edit.

3.    Press q to erase a function.

4.    Enter or edit the expression to define the function.

  • You may use functions and variables (including matrices and lists) in the expression. When the expression evaluates to a nonreal number, the value is not plotted; no error is returned.
  • You can access the shortcut menus by pressing b Ü - Ž.
  • In function mode the independent variable in the function is X. Func mode defines l as X. To enter X, press l or press b X.
  • When you enter the first character, the = is highlighted, indicating that the function is active.
  • As you enter the expression, it is stored to the variable Yn as a user-defined function in the Y= editor.

5.    Press = or the down arrow to move the cursor to the next function.

play video

Setting up the viewing window for a graph

Press d to access the window variables, which determine how the graph screen is displayed.

Play Video

Setting up the formatting options for the graph space

Press a  to access all the graph formatting options. This menu includes the options for points of interest trace, grid, and background color.

play video

Using the zoom features

Press f key to access the quick zoom options. Quick zoom options include the ZDecimal (default window), ZStandard, ZoomFit, and ZoomStat options.

play video

Exploring Points of Interest Trace

Press a  to access the Points of Interest Trace (POI) feature. It is on by default. POI allows graphical analysis while tracing a function including intersections of functions, minimums, maximums, the y-intercept and zeros.

Play video

Viewing and using the table

When a function is entered in the Y= editor, you can view a table of values by pressing a Ä.

Note: The table setup, a Á, determines how table values are displayed. Check the table setup values if the table results are not in expected fraction format. Using a mix of decimal and fractions will not retain fractions.