Solution 32011: Creating a .csv or .txt Class Roster for Import into the TI-Nspire CX Premium Teacher Software.
How do I create a class roster .csv or .txt for import into the TI-Nspire CX Premium Teacher Software?
Outlined below are guidelines to create a .csv or .txt file for import into the TI-Nspire CX Navigator:
First you will have to create either a .csv or .txt file with your class information populated. You can either create one from scratch or use the attached .csv or .txt files.
Please Note: To open .csv files you will need a spreadsheet program such as Microsoft® Excel® or OpenOffice® Calc if you do not have either of these programs it is suggested you use the .txt file.
If you create the files from scratch you will need to create a file with at least 4 columns with the below headers:
Class Name
First Name
Last Name
User Name
There are a few optional headers you can enter listed below:
Section Name
Student ID
Password
Specific information about the headers listed above can be found below:
•
Class Name corresponds to the name of the class the student is assigned
to, when clicking the class selector this is the name that will appear
in the list.
• First Name is the student’s first name
• Last Name is the student’s last name
•
User Name is the name the student will use to log in and must be unique
no two students in any of your classes can have the same username.
•
Section Name is appended to the end of the class name in the format
[Class Name] - [Section Name] this allows you to name your class names
the same and separate classes by their section.
• Student ID is a
numerical indicator assigned to each student and is only listed for
record keeping and is not used by the software in any way.
•
Password allows you to assign a specific password to a student rather
than having the student chooses their password when they first log in.
Once you have finished creating your .csv or .txt file you can import the class roster information using the steps in Solution 32012.
If you require additional assistance, please contact TI-Cares.