Education Technology

Modeling Exponential Decay with a Look at Asymptotes

Subject Area
Math: Algebra I: Exponential Functions
Level
9-12
Activity Time
90 Minutes
Software
TI Connect™
TI Calculator
TI-84 series
Other Materials
    This is Activity 6 from the EXPLORATIONS Book:
    A Hands-On Look at Algebra Functions: Activities for Transformation Graphing .

    The following materials are required for this activity:
  • Sets of 6-sided dice (numbered 1 - 6)
  • Alternate (non-standard) sets of dice
Resource Types
Lessons

Modeling Exponential Decay with a Look at Asymptotes

Activity Overview

In this activity, students approximate exponential decay models by defining parameters A and B in the exponential equation y = abx. They identify non-zero asymptote form of an exponential function.

Before the Activity

  • Set up the Transformation Graphing Application on the calculator using the TI Connect™ software
  • See the attached PDF file for detailed instructions for this activity
  • Print pages 54 - 61 the attached PDF file for the class
  • During the Activity

    Distribute the pages to the class.

    Follow the Activity procedures:

  • Roll around 36 dice and remove from the set any die that shows a 6 on its top face
  • Using only the dice left, repeat the step until no die remains or there have been 15 trials, whichever occurs first
  • Enter the number of rolls and number of dice left as lists
  • Plot the graph and select an appropriate value for A
  • Change the value of B to obtain a proper decay rate
  • Observe that the decaying curve does not reach zero, but tends to zero
  • Write the equation of the exponential function
  • Determine when y < 0.5, and when there are no dice left
  • Use the calculator to get a rough estimate of the location of the asymptote
  • Repeat experiment with non-standard set of dice
  • After the Activity

    Students' will complete the Student Worksheet and answer questions listed on it.

    Review student results:

  • As a class, discuss questions that appeared to be more challenging
  • Re-teach concepts as necessary
  • Subject Area
    Math: Algebra I: Exponential Functions
    Level
    9-12
    Activity Time
    90 Minutes
    Software
    TI Connect™
    TI Calculator
    TI-84 series
    Other Materials
      This is Activity 6 from the EXPLORATIONS Book:
      A Hands-On Look at Algebra Functions: Activities for Transformation Graphing .

      The following materials are required for this activity:
    • Sets of 6-sided dice (numbered 1 - 6)
    • Alternate (non-standard) sets of dice
    Resource Types
    Lessons
    iPad is a trademark of Apple Inc., registered in the U.S. and other countries.
    Vernier EasyData,Vernier EasyLink and Vernier EasyTemp are registered trademarks of Vernier Science Education.