Education Technology

Knowledge Base

Home | TI-Nspire™ Navigator

Solution 26870: Adding an Access Point for Use with the TI-Nspire™ Navigator™ System.

How do I add an Access Point to my computer so that I can use my TI-Nspire Navigator System?

The first step to setting up the TI-Nspire Navigator system hardware is to add the Access Point to the system. For help with adding the Access Point, follow the steps below:

1) First, open TI-Nspire Navigator Teacher Software then Network Manager by using your mouse to click [Tools] [Network Manager].

2) To verify if the Access Point is listed as [Connected] or [Detected] as shown in the image below.

If the Access Point status still shows as disconnected please visit Knowledgebase Article #26650.

If you need additional assistance with other components of the TI-Nspire Navigator System please visit Knowledgebase Article #30332.

If you require additional assistance please contact TI-Cares.