Knowledge Base
Solution 26650: Troubleshooting a TI-Nspire CX Navigator (TINAVAP3), TI-Nspire Navigator (TINAVAP2), and TI-Navigator (Nav-AP-US) Access Point That's Not Being Detected by a Computer.
How do I troubleshoot a Access Point that's not being detected by the computer?
To troubleshoot an Access Point (AP) that's not being detected by the computer verify the items below:
• TI-Navigator (Nav-AP-US) Only: Verify that the AP is connected to the AC Adapter and plugged into a valid power source. If plugged in correctly and working properly, the TI-Navigator should display a solid [Power] and a blinking [100 Link/Act] [Signal 802.11b/g] lights.
• Verify the USB cable that connects the AP to the computer is securely connected on both ends.
• Try connecting the USB cable to one of the computer's on-board USB ports and not a USB hub.
• Verify the computer's on-board USB port is working properly. To check this, disconnect the AP and try connecting a personal USB device (such as a cell phone or thumb drive) to the port being used by the AP. If the USB port detects the newly connected device, it is working properly.
After verifying the above items, please try the troubleshooting steps below to detect your AP:
• First try removing the power from the AP for about 10 seconds and reconnect the power and wait about 1 minute for the AP to detect using the steps below:
TI-Navigator (NAV-AP-US): Disconnect the AC Adapter.
TI-Nspire Navigator (TINAVAP2) and TI-Nspire CX Navigator (TINAVAP3): Disconnect the USB cable.
• TI-Navigator (NAV-AP-US) Only: Press the reset button located on the bottom of the AP for 5 seconds to reset the AP to default settings.
Windows Only:
If still not, detected try the additional troubleshooting steps below:
• Click [Windows]+[R] to open the run dialog and enter the text below then click [OK]:
appwiz.cpl
• Select the "TI-Nspire CX Premium Teacher Software" and select [Uninstall] and wait for the uninstall to complete.
• Click [Windows]+[R] to open the run dialog and enter the text below then click [OK]:
C:\Program Files\TI Education
• Delete the folders below if they still exist:
TI-Nspire CX Premium Teacher Software
TI-Nspire CX CAS Premium Teacher Software
• Next disconnect the AP from the computer.
• Download the EXE for the TI-Nspire CX Premium Teacher Software
• Reinstall the software by [Right Clicking] the EXE and selecting the option [Run as administrator].
• After it has installed launch the TI-Nspire CX Navigator Teacher Software and connect the AP to the computer and it should be detected in 2-5 minutes.
If still not detected manually install the driver using the steps below:
• Press [Windows key]+[R] to open the run dialog then type the text below in the dialog:
devmgmt.msc
• Click [OK] to launch the device manager.
• Connect the AP via USB and locate it under either under [Other Devices] or [Universal Serial Bus Controllers] it should have "AP" or "Navigator" in the name.
Please Note: After connecting it may take a few minutes for it to appear. The device manager will flash white when it detects a new device and refresh automatically.
• [Right Click] the device and choose the option [Update Driver]
• Choose the option [Browse my computer for driver software]
• Underneath [Search for drivers in this location:] and to the left of [Browse...] click the path listed then press [Ctrl]+[A] to select the path listed then [Backspace] to delete the path.
• Copy and paste the path below in this empty box:
C:\Program Files\TI Education\TI-Nspire CX Premium Teacher Software\drivers
• Make sure the checkbox [Include Subfolders] is checked then click [Next].
• The final screen will display the driver has installed correctly.
Please Note: If the driver install fails please verify if you have a ARM-based processor as a our software currently does not have a driver supported for ARM-based Windows computers:
• Click [Windows]+[I] to open the settings menu or click [Start] then search for "Settings" and open it when it is found in search.
• In the Settings menu click [System]
• In the System menu scroll through the options and click on [About]
• In the About menu look next to "System Type" and see if the text "ARM-based" is listed anywhere in the text listed. If this is listed then the driver is currently incompatible with your system.
macOS Only:
If still not, detected try the additional troubleshooting steps below:
• Update your macOS operating system to the latest version.
• If your macOS computer only has USB-C ports, use a USB-C to Micro-USB cable to connect your AP directly to your computer. If you need to purchase one, you can find them by searching the internet for “USB-C to Micro-USB cable”. Please also verify the cable you purchase supports data-transfer as some cables support charging only.
If you need additional assistance with other components of the TI-Nspire Navigator System please visit Knowledgebase Article #30332.
If you require additional assistance, please contact TI-Cares.