Education Technology

Solution 39258: Create a New TI-Nspire Navigator Class Database.

How do I create a new TI-Nspire Navigator class database?

To create a new TI-Nspire Navigator class database you would need to remove the existing database using the steps below:

Windows:

1) Close the TI-Nspire Navigator Teacher Software if it is open
2) Press [Windows key]+[R] to open the run dialog then type the text below in the dialog then click [OK]:

%localappdata%

3) In the above folder rename or delete the "Texas Instruments" folder which contains the TI-Nspire Navigator class database.

Mac:

1) Close the TI-Nspire Navigator Teacher Software if it is open
2) Launch [Finder] and then click [Go] [Go to Folder] and enter the text below then click [Go]:

~/Library/Application Support

3) In the above folder rename or delete the "Texas Instruments" folder which contains the TI-Nspire Navigator class database.