Education Technology

Knowledge Base

Home | TI-Innovator™ Technology

Solution 37817: What are the capabilities of the TI-Innovator™ Hub I/O Modules available from TI?

What are the capabilities of the TI-Innovator™ I/O Modules?

TI-Innovator Hub™ I/O Module Details

What are the capabilities of the TI-Innovator™ I/O Modules available from TI?

What are some examples of using the TI-Innovator™ I/O Modules available from TI?

What other I/O Modules could work with the TI-Innovator™ Hub?

The items contained in the TI-Innovator™ kits have all been verified to be fully compatible with the TI-Innovator™ system. The sketch of the TI-Innovator™ Hub can support other modules that are compatible with the universal 4-pin connector that is used for the input and output ports. Supported commands and potential modules are listed below. If there are specific components you think would be valuable for classroom activities, please contact TI-Cares and provide your feedback.

Please Note: Texas Instruments Customer Support is available to answer questions about the products that are sold directly through our Educational Products Dealers or the TI Online Store. For components purchased elsewhere, such as those listed below, please refer to the manufacturer or point of purchase for technical support.

Example Module Component(s)

Command/Sketch Object

Barometer Sensor

BAROMETER

Button, Magnetic Switch

BUTTON

3-Axis Digital Compass

COMPASS

Fan

DCMOTOR

Temperature & Humidity Sensor

DHT

Single or variable color LEDs

LED

Light sensor

LIGHTLEVEL

Sound Sensor, Loudness Sensor

LOUDNESS

Moisture Sensor

MOISTURE

Collision Sensor

MOTION

PIR Motion Sensor

MOTION

Slide Potentiometer

POTENTIOMETER

Rotary Angle Sensor

POTENTIOMETER

Electromagnet, Relay

RELAY

Servo Motor

SERVO

Buzzer, speaker

SPEAKER

Switch

SWITCH

Temperature Sensor

TEMPERATURE