Education Technology

Solution 34913: Correcting the "WINDOW RANGE" Error When Graphing on the TI-83 Plus and TI-84 Plus Family of Graphing Calculators. 

How do I correct the WINDOW RANGE error when graphing on the TI-83 Plus and TI-84 Plus family of graphing calculators?

If the WINDOW RANGE error is returned when graphing this means the values for the WINDOW settings need to be adjusted.



To correct the WINDOW RANGE error, the default WINDOW values will need to be restored using the ZStandard (ZoomStandard) command (see steps below):

1) Press [ZOOM].
2) Scroll down to 6:ZStandard and press [ENTER].

The default settings for the WINDOW values are:



Please see the TI-83 Plus and TI-84 Plus Family guidebooks for additional information.