Education Technology

Solution 34512: Entering Numbers Using Scientific Notation on a TI-84 Plus C Silver Edition.

How do I enter numbers using scientific notation on a TI-84 Plus C Silver Edition?

The EE function is used to enter numbers in scientific notation on a TI-84 Plus C Silver Edition.

NOTE: EE is used to represent "times 10 to the power of".

Example: Input 3.5 x 106 and display the results in standard form.

Solution:

• Press [3] [.] [5].
• Press [2ND] [EE].
• Press [6] [ENTER].



Please see the TI-84 Plus C Silver Edition guidebook for additional information.