Knowledge Base
Solution 13061: Basics Steps for Creating Text Files Using the NoteFolio™ Creator Software.
How can I use the TI NoteFolio Creator software to create text files for my calculator?
The steps below show how to create text files and transfer them to the calculator using the NoteFolio Creator software.
1) Install TI Connect™ and TI NoteFolio™ Creator on the computer.
2) Install the NoteFolio application on the calculator.
3) Restart the computer.
4) Start TI NoteFolio Creator.
5) Select New NoteFolio™ folio and select the calculator type.
6) Click OK.
7) Type the text or paste it from another application.
8) Connect the calculator to the computer.
9) Click Send to Device
10) A window will appear requesting a file name. Type the name and click OK.
Please Note: A Select Calculator window may appear If so, when the correct calculator model shows, click Select and the text will transfer to the calculator
Another option is to type the text in Microsoft® Word and send it directly to the calculator.
1) Open MS Word
2) Type the text you wish to send or paste it from another application
3) Connect the calculator to the computer
4) Click TI Tools >>TI NoteFolio Creator >> Send to Device
Please Note: A Select Calculator window may appear If so, when the correct calculator model shows, click Select and the text will transfer to the calculator
Please see the TI-NoteFolio Creator guidebook for additional information.