Education Technology

Solution 15345: Converting Temperatures Between Celsius and Fahrenheit on the TI-36X Solar.

How can I convert temperatures between Celsius and Fahrenheit on the TI-36X Solar?

The following example describes how to convert temperatures from Celsius to Fahrenheit on the TI-36X Solar:


Convert 37° Celsius to Fahrenheit:

Please be aware that the °C formula is as follows:

°C = (°F-32) x (5/9).

• Press [3] [7] [2nd] [►° F].
• The screen will display 98.6°F.

The following example below describes how to convert temperatures from Fahrenheit to Celsius:

Convert 100° Fahrenheit to Celsius:

• Press [1] [0] [0] [3rd] [► °C].
• The screen will display 37.78°C.

Please see the TI-36X Solar guidebook for additional information.