Education Technology

Solution 12299: Using the Percent Key on the TI-30X IIS/B and TI-34 II Explorer Plus™.

How do I use the percent key on the TI-30X IIS/B and TI-34 II Explorer Plus?

The example below will demonstrate using the percent key in an operation on the TI-30X IIS/B, and the TI-34 II Explorer Plus.

Example: 50 + 50% of 50 = ?

• Input 50 [+] 50 [2nd] [(], then [(] 50 [)].
• Press the [=] key to compute.

The answer is 75.

Please see the TI-30X IIS/B and TI-34 II Explorer Plus guidebooks for additional information.