Linear Equation Investigation
Linear Equation Investigation
Students are given a real-life situation (cost of a birthday party) they must create an algebraic equation, table of values, and a scatterplot of the table that is created. They are asked to explain patterns that they observed in each type of representation and also check their accuracy when creating the graph.
Teacher preparation:
Complete the activity to prepare yourself for the discussion that may take place in regards to the equation used, where the values in the numerical table should end and begin as well as the difference between discrete and continuous data in case the question is asked.
I suggest completing this activity as a final assignment for investigating linear equations. There are a lot of concepts that are investigated in this activity. Students should feel comfortable with creating a scatter plot from a table of values.
This activity is to be used as a tool that links an equation, table, and scatter plot together in a summary format in regards to a linear relationship.
Summary and Extension question packet can be assigned as homework to wrap up the investigation. Students do not need the hand held to complete this packet
Before the Activity Files
During the Activity Files
After the Activity Files
Vernier EasyData,Vernier EasyLink and Vernier EasyTemp are registered trademarks of Vernier Science Education.