Center and Spread
TI-Nspire™ CX CAS
Center and Spread
Students will recognize that the mean and standard deviation (SD) and the median and interquartile range (IQR) are two ways to measure center and spread.
- Students will recognize that the mean and standard deviation (SD) and the median and interquartile range (IQR) are two ways to measure center and spread.
- Students will recognize that in a skewed distribution the mean is pulled in the direction of the tail, and the standard deviation is increased; in a distribution with an outlier, the mean is pulled in the direction of the outlier, and the standard deviation is increased.
- Students will be able to illustrate that the median and IQR are resistant to skewness/outliers while the mean and standard deviation are not.
- Students will recognize that the median and IQR are preferred when a distribution is skewed while either mean and SD or median/IQR are acceptable for approximately symmetric distributions.
- Bimodal or unimodal
- Interquartile range
- Mean, median, and standard deviation
- Outlier
- Resistant
- Akewed or symmetric distribution
This lesson involves moving points on dotplots. Students will:
- change the shape of the distribution and notice the effect on the mean and median and on the standard deviation and IQR.
- drag points to compare the effect of outliers on the mean/standard deviation and median/IQR.
- make and justify a conjecture about which measures are preferred based on the shape of the distribution.
TI-Nspire™ CX CAS
Vernier EasyData,Vernier EasyLink and Vernier EasyTemp are registered trademarks of Vernier Science Education.