Solution 34603: Finding the X-Intercept of a Function on the TI-83 Plus and TI-84 Plus Family of Graphing Calculators.
How can I find the x-intercepts of a function on the TI-83 Plus and TI-84 Plus family of graphing calculators?
To find the x-intercepts of a function, the zero command must be used. Follow the example below for help with using the zero command.Example: 2X - 7
1) Press [Y=] to access the Y= Editor.
2) Press [Clear] then [2] [X,T,θ,n] [-] [7]
3) Press [zoom] then [5] to graph the function and select standard viewing window.
![](https://education.ti.com/images/kbase/c34603ss1.bmp)
![](https://education.ti.com/images/kbase/c34603ss2.bmp)
4) Press [2nd] then [trace] to access the CALCULATE menu
5) Press [2] to select the zero command.
6) "Left Bound?" will be displayed, select a point on the graph that is to the left of the x-intercept by using the [←] or [→] keys.
7) Once selected press [enter] to mark this as the Left Bound.
![](https://education.ti.com/images/kbase/c34603ss3.bmp)
8) "Right Bound?" will be displayed, select a point on the graph that is to the right of the x-intercept using the [←] or [→] keys.
9) Once selected press [enter] to mark this as the Right Bound.
![](https://education.ti.com/images/kbase/c34603ss4.bmp)
10) "Guess?" will be displayed using the [←] or [→] keys, move the cursor until it is close to or directly on the x-intercept
11) Press [enter] to submit your Guess and display the exact point of the x-intercept which is (3.5,0)
![](https://education.ti.com/images/kbase/c34603ss5.bmp)
![](https://education.ti.com/images/kbase/c34603ss6.bmp)
Please see the TI-83 Plus and TI-84 Plus Family guidebooks for additional information.
Last updated: 7/24/2023