Solution 34495: Converting Mixed Numbers to Improper Fractions on the TI-84 Plus Family of Graphing Calculators.
How do I convert mixed numbers to improper fractions (and vice versa) on the TI-84 Plus family of graphing calculators?
To convert mixed numbers to improper fractions (and vice versa) using the TI-84 Plus family of graphing calculators, follow the examples below.
For Example: Convert 1 3/5 to an improper fraction.
1) Press [ALPHA] [Y=] to access the FRAC menu.
2) Press [2] to select the Un/d function.
3) Input 1 and press [Right Arrow]
4) Input 3 and press [Down Arrow].
5) Input 5 and press [Right Arrow] [ENTER].

For Example: Convert 9/6 to a mixed number.
1) Press [ALPHA] [Y=] to access the FRAC menu.
2) Press [1] to select the n/d function.
3) Input 9 and press [Down Arrow].
4) Input 6 and press [Right Arrow].
5) Press [ALPHA] [Y=].
6) Press [3] to select the >n/d<>Un/d function.
7) Press [ENTER].

Please see the TI-84 Plus Family guidebooks for additional information.
Last updated: 7/30/2024