Education Technology

Solution 11973: Viewing Text Files on the TI-83 Plus and TI-84 Plus.

How can I view text files on a TI-83 Plus and TI-84 Plus?

With the NoteFolio™ Flash App installed on a compatible TI graphing calculator, it is possible to create, as well as open and view saved text files.  Follow the procedure below to open up a text file in NoteFolio:

1) Press the [APPS] key to go to the APPLICATIONS menu.
2) Press [↓] until NoteFolio is selected, then press [ENTER] [ENTER].
3) Press the [GRAPH] key to display the MENU.
4) Press [2] to select open - the names of all the text files that are stored on the device are displayed.
5) Press [↓] to select the file to be opened and press [ENTER] - the text is displayed, and the file name is shown in the bottom-left corner of the NoteFolio screen.

Please Note: The NoteFolio application is not available for the TI-84 Evo, TI-84 Plus CE or TI-84 Plus C Silver Edition.

For additional information on using NoteFolio, refer to the online guidebook for the App.