Education Technology

Solution 12666: Locating a Graphing Calculator's Unique Product ID Number.

Each TI Flash-based graphing calculator has a distinct product ID number. These units are listed below:

• TI-73 Explorer™
• TI-83 Plus
• TI-84 Plus
• TI-84 Plus C Silver Edition
• TI-84 Plus CE
• TI-84 Evo
• TI-89
• TI-89 Titanium
• TI-92 Plus
• Voyage™ 200

Procedure for Locating Product ID on the TI-73 Explorer, TI-84 Plus, TI-84 Plus C Silver Edition, TI-84 Plus CE, and TI-84 Evo:

• Press [ON]
• Press [2nd]
• Press [+] (notice the word "MEM" written above the key)

• Press [1] ("About")

The 14-digit product ID# should now be displayed.

Procedure for Locating the Product ID on the TI-89, TI-89 Titanium, TI-92 Plus, and Voyage 200:

• Press [ON]
• Press [F1]
• Highlight "About"

• Press [ENTER]

The14-digit product ID# should now be displayed.

Procedure for Locating the Product ID using TI Connect™

• Open TI Connect.
• With the calculator connected to the TI Connectivity Cable, open Device Info.
• Device Info will poll the calculator for information and display it in the Device Info dialog.

The calculator ID will be displayed as Device ID. From here, you can save the information by clicking file and choosing save. This will save the information into a standard text document (.txt file) which can be read by a variety of programs.

Also, the ID List tab displays IDs associated to that calculator. From here, the IDs can be copied and pasted into any Windows® program.

Please see the guidebooks for additional information