Solution 11500: Resolving the "Error retrieving data from the selected file" Message when Transferring a Program File Using the TI Connect™ Software for Windows®.
How do I fix the "Error retrieving data from the selected file" message when transferring a program file using TI Connect?
To resolve the "Error retrieving data from the selected file" message when transferring a program, the latest version of the TI Connect software will need to be installed. Please refer to the instructions below to un-install the TI Connect software from the computer:
• Disconnect the TI Connectivity Cable from the computer.
• Go to Start >> Control Panel or Start >> Settings >> Control Panel and select the option "Add or Remove Programs".
• Scroll through the list of installed programs and locate the TI Connect software.
• Click on the TI Connect software from the list of installed programs and select the "Remove" option.
Once the un-install process has completed, re-start the computer and install the latest version of the TI Connect software.