Solution 12652: Decimal Degrees (DD) to Degrees, Minutes, Seconds (DMS) Conversions on the TI-81.
How do I perform decimal degrees (DD) to degrees, minutes, seconds (DMS) conversions on the TI-81?
The TI-81 does not have built-in DMS-DD conversion features. However, these features can be added to the graphing calculator with the following programs.1. The following program adds DMS to decimal degrees conversions to the TI-81:
Prgm1:DMS
:Disp "DEGREE"
:Input D
:Disp "MINUTES"
:Input M
:Disp "SECONDS"
:Input S
:D+M/60+S/3600->D
:Disp D
2. The following program adds decimal degrees into DMS conversions to the TI-81:
Prgm2:DD
:Disp "DECIMAL DEGREE"
:Input I
:IPart I->D
:(FPart I)*60->M
:IPart ((FPart M)*60)->S
:IPart M->M
:D+M/100+S/1000->D
:Disp D