Simple Ionic Compounds
Simple Ionic Compounds
In this lesson students will review and test their understanding of simple ionic compounds.
Start lesson by reviewing notes: Ionic Compounds these are compounds composed of metals and nonmetals ionic compounds are held together by ionic bonds this type of bonding involves a complete transfer of electrons from metallic atoms to nonmetallic atoms Ex. Ionic bonds within lithium fluoride unlike molecular compounds in which atoms bond covalently to form "well-defined" units know as molecules, ionic compounds form formula units Binary Ionic Compounds These are compounds composed of 2 different ions (metallic + nonmetallic) To write the name of a binary ionic compound: 1) name of first element 2) name of second element, ending change to ide * prefixes are NOT used in name of binary ionic compounds Ex. Li3N MgCl2 Al2S3 To write the name for a binary ionic compound: 1) determine the charge of each ion 2) balance charges by changing the number of each ion (subscript) Ex. Determine the formula for the compound sodium oxide 1) Determine if the compound is ionic or molecular 2) If the compound is ionic determine the charge of each ion 3) Balance the charges
Quick Poll Get the students to find the determine the chemical formulas for the following compounds, ask then to just enter the number of each atom in the compound separated a comma. Ex 1. sodium bromide Ex 2. potassium sulfide Ex 3. barium chloride Ex 4. calcium nitride Learning Check Send learning check file to students allow 15 minutes to finish quiz.
Force collect from class analysis and then review in class analysis slide show. Extension Questions: Lead into the next topic of multi-valent compounds by asking students to balance the following examples in learning check. Ex 1 iron nitride Ex 2 vanadium sulfide Ex 3 molybdenum phosphide Ex 4 copper chloride
Vernier EasyData,Vernier EasyLink and Vernier EasyTemp are registered trademarks of Vernier Science Education.