TI-89 Titanium Graphing Calculator Lesson
Module 16: The Fundamental Theorem of Calculus
Introduction | Lesson 1 | Lesson 2 | Lesson 3 | Self-Test
Lesson 16.3: The Fundamental Theorem of Calculus
A restatement of the Fundamental Theorem of Calculus is presented in this lesson along with a corollary that is used to find the value of a definite integral analytically.
Restating the Fundamental Theorem
You have discovered the Fundamental Theorem in the context of finding areas under a curve but a more general version of this theorem can be proved without an appeal to area. The following is a restatement of the Fundamental Theorem.
If f is continuous on [a, b], then the function
has a derivative at every point in [a, b], and the derivative is
That is, the derivative of a definite integral of f whose upper limit is the variable x and whose lower limit is the constant a equals the function f evaluated at x. This is true regardless of the value of the lower limit a. The function named F is the same as the area function that was previously explored.
Using the Restated Fundamental Theorem
- Set Angle mode to Radian
- Execute NewProb from the Clean Up menu
16.3.1 Use the restatement of the Fundament theorem to evaluate the following derivatives, then check your predictions with the TI-89.
Click here for the answer.
16.3.2 Predict the following derivative. Check your answer with the TI-89. Hint: You will have to use the chain rule.
Click here for the answer.
16.3.3 Evaluate the following derivative and check with your TI-89.
Click here for the answer.
16.3.4 Find a more general version of the Fundamental theorem by predicting the following derivative. Check your work with the TI-89.
The function F is called an antiderivative of the function f.
16.3.5 Use the corollary to predict the value of
, then check your work with the TI-89.
Click here for the answer.
16.3.6 Use the corollary of the Fundamental theorem to evaluate
then check your work with your calculator.
Click here for the answer.