Knowledge Base
Solution 30211: Computing Net Present Value (NPV), Modified Internal rate (MIRR), and Internal Rate of Return (IRR) Using a TI-Nspire™ Family Products.
How do I compute NPV, MIRR, and IRR using a TI-NSPIRE family handheld or software?
Commands Syntax.mirr(financeRate,reinvestRate,CF0,CFList[,CFFreq])
npv(InterestRate,CFO,CFList[,CFFreq])
irr(CF0,CFList [,CFFreq])
CF0 is the initial cash flow at time 0; it must be a real number.
CFList is a list of cash flow amounts after the initial cash flow CF0.
CFFreq is a list in which each element specifies the frequency of occurrence for a rouped (consecutive) cash flow amount, which is the corresponding element of CFList. The default is 1; if you enter values, they must be positive integers < 10,000.

The following examples will demonstrate how to compute NPV, MIRR, and IRR.
For example:
Initial cash flow is -100
Interest rate is 7%
Cf1=10 Frequency=2
CF2=-9 Frequency=3
CF3=20 Frequency=5
What is the NPV, MIRR, and IRR?
1) Press [Home] and select Lists & Spreadsheets.
2) Press [10] [enter] [-9] [enter] [20] [enter] [Ctrl] [7].
3) Press [Tab] [k] [Tab] [l] [enter] [Tab].
4) Press [2] [enter] [3] [enter] [5] [enter]
5) Press [Home] and select Calculator
Calculate NPV:
1) Press [menu] [8: Finance] [4: Cash Flows] [1: Net Present Value]
2) Press [7] [,] [-] [1] [0] [0] [,] [k] [,] [l] [Enter]

Calculate IRR:
1) Press [menu] [8: Finance] [4: Cash Flows] [2: Internal Rate of Return]
2) Press [-] [1] [0] [0] [,] [k] [,] [l] [Enter]

Calculate MIRR:
1) Press [menu] [8: Finance] [4: Cash Flows] [3: Modified Internal Rate of Return]
2) Press [i] [r] [r] [(] [-] [1] [0] [0] [,] [k] [,] [l] [Right Arrow] [,] [7] [,] [-] [1] [0] [0] [,] [k] [,] [l] [Enter]
Please Note: You can alternatively copy the IRR result by pressing [Up Arrow] then [Enter] instead of computing the value within MIRR if you computed IRR before MIRR as listed in the image below.

Please see the TI-Nspire CX, TI-Nspire CX CAS, TI-Nspire and TI-Nspire CAS guidebooks for additional information.