Education Technology

Knowledge Base

Home | TI-Innovator™ Technology

Solution 37798: What connection ports are available on the TI-Innovator™ Hub, and what can they connect to?

TI-Innovator™ Hub Port Information.

What connection ports are available on the TI-Innovator™ Hub, and what can they connect to?

3 input ports: Used to communicate and gather data from input modules:

  • IN 1 and IN 2 are for 3.3V sensors. (most sensors are 3.3V sensors)
  • IN 3 is for 5V sensors.
  • Most sensors will work in any of the ports. (i.e., a 3.3V sensor will not get damaged if used with IN 3, but the readings may not be accurate)

3 output ports: Used to control output modules:

  • OUT 1 and OUT 2 are for use with modules requiring 3.3V.
  • OUT 3 is for use with modules requiring 5V, such as motors.

Breadboard connector: Twenty (20) receptacle pins for communication with components on a breadboard:

  • The top row is for the signals and can be addressed in the programs using the “BB1..BB10” names.
  • The first 8 pins on the bottom provide a ‘ground’ path for the circuit.
  • The two other pins provide power – 3.3V and 5V.

I2C connector:

This port is for future capability, will connect to peripherals that use the I2C communication protocol.

What is the difference between the two USB ports?

DATA: This is a mini-USB port, labeled “DATA B”, that is used to connect to the TI graphing calculator, or a computer running TI-Nspire™ CX software. The USB port is located on the same side as the Light Sensor.

POWER: This USB port, labeled “PWR,” is located on the same side as the Breadboard connector.

This is a micro-USB port that is used for two purposes:

1) Connect to external power source (TI Wall Adapter and TI-Innovator™ External Battery) when using components that require 5V (e.g.: motor).
2) Connect to computer USB port to update the TI-Innovator™ Sketch.