Solution 34711: Troubleshooting Error: Archived on the TI-84 Plus C Silver Edition Graphing Calculator.
How is the Error: Archived corrected on the TI-84 Plus C Silver Edition Graphing Calculator?
When attempting to use a program, variable, or any data such as lists it is possible to get the following error message.:
This may be received when attempting to use something that is archived in the calculator's memory. The following steps can be used to unarchive it using the Memory Management editor:
1) Press [2ND] [MEM] [2].
2) Press [1].
3) Locate the program or data to be unarchived, this will be identifiable with an asterisk to the left of the file name.
4) Place the cursor by it.
5) Press [ENTER].
Once the asterisk has disappeared, the program, variable, or data has become unarchived.
Try executing the program or using the variable or data.
Please Note: Applications always have an asterisk next to their name and this asterisk cannot be removed. Applications reside in the Archive memory and can be run from there, unarchiving all of the data may help to determine what is potentially being referenced in the program.