Solution 34535: Creating Strings on the TI-84 Plus C Silver Edition Graphing Calculator.
How can I create a string variable on the TI-84 Plus C Silver Edition graphing calculator?
A string is a sequence of characters enclosed within quotation marks. Characters are the units combined to form a string. Each number, letter, and space is one character. Each instruction or function, such as sin( or tan( is one character. Quotation marks do not count as string characters.
To enter a string on a blank line on the Home screen or in a program:
• Press [ALPHA]["] to indicate the beginning of the string.
• Enter the string text (this may include number, letters, functions, instructions, or spaces).
• Press [ALPHA]["].
• Press [ENTER].
The TI-84 Plus C Silver Edition has 10 built-in variables to which strings can be stored. Other variables cannot be used to store strings. To store a string to a string variable:
• Press [ALPHA]["] to indicate the beginning of the string.
• Enter the string text.
• Press [ALPHA]["] to indicate the end of the string.
• Press the [STO->] key.
• Press [VARS] to display the VARS menu.
• Move the cursor to 7:String.
• Press the [ENTER] to display the STRING secondary menu.
• Select the string variable from str1 to str0 to which to store the string.
• Press [ENTER].
Please Note: To display the contents of a string variable on the home screen, select the string variable from the VARS STRING menu, and then press [ENTER].

Please see the TI-84 Plus C Silver Edition guidebook for additional information.