Education Technology

Solution 12784: Use of the Max() Function on the TI-89 family, TI-92 Plus, and Voyage™ 200.

How can I use the max() function on the TI-89 family, TI-92 Plus and Voyage 200?

The max() function returns the maximum of the two arguments. If the arguments are two lists or matrices, it returns a list or matrix containing the maximum value of each pair of corresponding elements. The syntax for this command is max(expression, expression), max(list1, list2) or max(matrix 1, matrix 2). For example:

Please see the TI-89 family, TI-92 family and Voyage 200 guidebooks for additional information.