Education Technology

Knowledge Base

Home | All other products

Solution 10250: Charging a TI-Navigator™ Type I or Type II Hub with a Power Adapter.

Can the power adapter that came along with my TI-Navigator system be used to charge a TI-Navigator Type I or Type II Hub?

Yes, the power adapter that came along with the TI-Navigator system can be used to charge a TI-Navigator Type I or Type II Hub. Take special care to ensure no other power adapter is used except the power adapter packaged with the system. Using any other power adapter (i.e. a laptop adapter) could damage the hub. If more hubs (4 maximum) need to be charged at once, the TI-Navigator Charging Bay should be used.

For TI-Navigator Type I Hubs, which are blue, please use the power adapter A/C 9930 that came along with the TI-Navigator Type I system. For more information on a TI-Navigator Type I system, take a look at the TI-Navigator Getting Started Poster.

For TI-Navigator Type II Hubs, which are light-gray, please use the power adapter A/C 9926 that came along with the TI-Navigator Type II system. For more information on a TI-Navigator Type II system, take a look at the TI-Navigator Installation Guide.

For information on the difference between charging hubs with the TI-Navigator Charging Bay versus charging a hub with the power adapter, take a look at the case titled Charging Bay Verses Power Adapter with TI-Navigator Type I and Type II Hubs.