Education Technology

Solution 39518: Compatibility of Programs Written for the TI-83 Plus, TI-84 Plus and TI-84 Plus C Silver Edition Running on the TI-84 Plus CE.

Can I run programs written for TI-83 Plus, TI-84 Plus family and TI-84 Plus C Silver Edition on the TI-84 Plus CE?

Some TI Basic programs for the TI-83 Plus and TI-84 Plus will run on the TI-84 Plus CE.

Please Note: Many Programs will have to be modified for writing to the graph area as the resolution of the TI-84 Plus CE is higher then the TI-83 Plus and TI-84 Plus.

TI-84 Plus C Silver Edition Programs should work on the TI-84 Plus CE as the resolution is the same.

Assembly programs will not work on the TI-84 Plus CE because of changes in how assembly programs are run please see KB#39498

Please see the TI-84 Plus CE guidebook for additional information.