Education Technology

Solution 15401: Maximum Number of Digits in Entry Line on the TI-30X IIS/B and TI-30XS MultiView™ Scientific Calculators.

How many digits can be entered in the entry line on the TI-30X IIS/B and TI-30XS MultiView?

The entry line of the TI-30X II/B calculator can contain up to 88 characters. The entry line of the TI-30XS MultiView calculator can contain up to 80 characters.


When the <-- or --> appears in the display, the entry line contains more characters to the left or right. When up or down arrows appears, more characters are located above or below the entry line.

Please see the TI-30X IIS/B or TI-30XS MultiView guidebooks for additional information.