Education Technology

Solution 28632: Converting from Degrees Celsius to Fahrenheit on the TI-73 Explorer™.

How do I convert from degrees Celsius to Fahrenheit on a TI-73 Explorer?

To convert degrees from Celsius to Fahrenheit, use the unit converter.

Example:

Convert 32 degrees Celsius to degrees Fahrenheit.

• Press [3],[2], [2nd] [Convert]

• Scroll down using the down arrow and select [5: Temp...], [ENTER]

• Select [1:degC], [Enter]
• Select [2:degF], [Enter]
• Press [Enter]

Answer is 89.6

More information is available in the TI-73 Explorer guidebook.